<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 How I can disconnect OpenSDA debug module on FRDM-KL05Z?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-I-can-disconnect-OpenSDA-debug-module-on-FRDM-KL05Z/m-p/360943#M18314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I remove R28 to disconnect the debugging module, but the microcontroller does not work. And if I put the J5 jummper works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to disconnect the debugging module to consume less current.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Feb 2015 19:04:31 GMT</pubDate>
    <dc:creator>OmarIsaiPinales</dc:creator>
    <dc:date>2015-02-09T19:04:31Z</dc:date>
    <item>
      <title>How I can disconnect OpenSDA debug module on FRDM-KL05Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-I-can-disconnect-OpenSDA-debug-module-on-FRDM-KL05Z/m-p/360943#M18314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I remove R28 to disconnect the debugging module, but the microcontroller does not work. And if I put the J5 jummper works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to disconnect the debugging module to consume less current.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 19:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-I-can-disconnect-OpenSDA-debug-module-on-FRDM-KL05Z/m-p/360943#M18314</guid>
      <dc:creator>OmarIsaiPinales</dc:creator>
      <dc:date>2015-02-09T19:04:31Z</dc:date>
    </item>
    <item>
      <title>Re: How I can disconnect OpenSDA debug module on FRDM-KL05Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-I-can-disconnect-OpenSDA-debug-module-on-FRDM-KL05Z/m-p/360944#M18315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do a test with FRDM-KL05Z board, the KL05 will work with R28 removed and jumper J4 be shuttled (J5 jumper is open).&lt;/P&gt;&lt;P&gt;For the OpenSDA K20 chip pin6 VREGIN connects with OPENSDA USB VBUS, P3V3_USBSER will with 1.5V voltage.&lt;/P&gt;&lt;P&gt;I recommend customer to use external DC power supply, add 3.3v to jumper 4 and short J9-3 with J9-4.&lt;/P&gt;&lt;P&gt;The reason is for RST_TGTMCU pin connects with K20's pin21, which default function is ADC0_SE9.&lt;/P&gt;&lt;P&gt;The ADC input pin as voltage divide resistor and KL05 reset pin voltage will divide to 1.3V and KL05 will be in reset state.&lt;/P&gt;&lt;P&gt;So short J9-3 and J9-4 will pull up the KL05 reset pin to 3.3V and KL05 could work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 02:07:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-I-can-disconnect-OpenSDA-debug-module-on-FRDM-KL05Z/m-p/360944#M18315</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-02-11T02:07:12Z</dc:date>
    </item>
  </channel>
</rss>