<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: TWR-K60F120M + TWR-SER - Setup issues</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-TWR-SER-Setup-issues/m-p/359170#M18123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48445i3B339CD1E2EAFD98/image-size/large?v=v2&amp;amp;px=999" title="Successful Firmware Upgrade.jpg" alt="Successful Firmware Upgrade.jpg" /&gt;&lt;/span&gt;If it helps, the firmware of the uC has been successfully updated as can be seen here...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Dec 2014 20:14:25 GMT</pubDate>
    <dc:creator>cramful</dc:creator>
    <dc:date>2014-12-17T20:14:25Z</dc:date>
    <item>
      <title>TWR-K60F120M + TWR-SER - Setup issues</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-TWR-SER-Setup-issues/m-p/359169#M18122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am having trouble running the "Accelerator Demo Application v 2.10".&amp;nbsp; When I tilt the tower, my mouse tracks the accelerometer output!&amp;nbsp; I do not see anything on the graph intended for the purpose. I think the "virtual serial" port is not properly installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run the demo, the "USB COM" port fails to open.&amp;nbsp; In the "Device Manager" panel, I instead opened COM6 and that is when my mouse starts responding to the tower tilt angle.&amp;nbsp; I know that the device under COM6 should appear under the "JUNGO" title but...&amp;nbsp;&amp;nbsp; I have uninstalled and re-installed the "pemicro_osbdm_osjtag_tower_toolkit" several times but I am stuck with&amp;nbsp; the same issue.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48431i53A62D9BF915871D/image-size/large?v=v2&amp;amp;px=999" title="COM Port Mapping.jpg" alt="COM Port Mapping.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I am running Windows 7 Professional.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also tried using the DB9 connector and COM4 (COM1 used with something else) after disconnecting the USB cable from TWR-SER.&amp;nbsp; No response at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions would be most welcome. :smileyconfused:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chundra&lt;/P&gt;&lt;P&gt;======&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2014 17:08:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-TWR-SER-Setup-issues/m-p/359169#M18122</guid>
      <dc:creator>cramful</dc:creator>
      <dc:date>2014-12-17T17:08:54Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60F120M + TWR-SER - Setup issues</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-TWR-SER-Setup-issues/m-p/359170#M18123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48445i3B339CD1E2EAFD98/image-size/large?v=v2&amp;amp;px=999" title="Successful Firmware Upgrade.jpg" alt="Successful Firmware Upgrade.jpg" /&gt;&lt;/span&gt;If it helps, the firmware of the uC has been successfully updated as can be seen here...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2014 20:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-TWR-SER-Setup-issues/m-p/359170#M18123</guid>
      <dc:creator>cramful</dc:creator>
      <dc:date>2014-12-17T20:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60F120M + TWR-SER - Setup issues</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-TWR-SER-Setup-issues/m-p/359171#M18124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is an error message I obtained at one point.&amp;nbsp; Does it help to debug the issue which has still not been resolved?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48507i20CBD26499B89C72/image-size/large?v=v2&amp;amp;px=999" title="TWR-K60F120M - Error Message.png" alt="TWR-K60F120M - Error Message.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Dec 2014 20:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-TWR-SER-Setup-issues/m-p/359171#M18124</guid>
      <dc:creator>cramful</dc:creator>
      <dc:date>2014-12-18T20:10:47Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60F120M + TWR-SER - Setup issues</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-TWR-SER-Setup-issues/m-p/359172#M18125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chundra Ramful:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the time with no response. Are you still having issues?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the pictures above it seems that the OSBDM interface can be upgraded and works as expected. But then you mentioned the &lt;STRONG&gt;Accelerator Demo Application v 2.10&lt;/STRONG&gt;. I am not sure what application you are referring to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are still experiencing problems, please share the current status and more details about the specific issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 04:32:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-TWR-SER-Setup-issues/m-p/359172#M18125</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-02-03T04:32:54Z</dc:date>
    </item>
  </channel>
</rss>