<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: different chipselect selection for SPI</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357550#M17932</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is what I see.&amp;nbsp; In section 3.9.4.3 of the K60 Reference Manual:&lt;/P&gt;&lt;P&gt;This device supports two CTARs on all instances of the SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you have two sets of control-timing you can select between (&lt;STRONG&gt;SPIx_CTAR0 &amp;amp; &lt;STRONG&gt;SPIx_CTAR1) &lt;/STRONG&gt;&lt;/STRONG&gt;for each SPIx_PUSHR operation, which may indeed be 'fewer' than the available CS selections in a SPI instantiation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Mar 2015 21:53:47 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2015-03-05T21:53:47Z</dc:date>
    <item>
      <title>different chipselect selection for SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357546#M17928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hai sir,&lt;/P&gt;&lt;P&gt;i am using K60 tower board .if i am using different chipselect how to set baudrate,cpol,cpha for different chipselect.&lt;/P&gt;&lt;P&gt;there is only one register for baudrate select. so each time at running state i cant chenge this regiser so how to set for different chip select&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 13:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357546#M17928</guid>
      <dc:creator>lijofrancis</dc:creator>
      <dc:date>2015-03-04T13:56:21Z</dc:date>
    </item>
    <item>
      <title>Re: different chipselect selection for SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357547#M17929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The chip select is controlled by the value in the &lt;STRONG&gt;SPIn_PUSHR&lt;/STRONG&gt; register so you can control the CS used on a byte basis.&lt;/P&gt;&lt;P&gt;The CS setting in &lt;STRONG&gt;SPIn_MSR&lt;/STRONG&gt; controls whether it is active '0' or active '1' but not how it is actually used when sending data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;K60: &lt;A href="http://www.utasker.com/kinetis/TWR-K60N512.html" title="http://www.utasker.com/kinetis/TWR-K60N512.html"&gt;µTasker Kinetis TWR-K60N512 support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/TWR-K60D100M.html" title="http://www.utasker.com/kinetis/TWR-K60D100M.html"&gt;µTasker Kinetis TWR-K60D100M support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/TWR-K60F120M.html" title="http://www.utasker.com/kinetis/TWR-K60F120M.html"&gt;µTasker Kinetis TWR-K60F120M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 15:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357547#M17929</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-03-04T15:22:22Z</dc:date>
    </item>
    <item>
      <title>Re: different chipselect selection for SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357548#M17930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lijo Francis:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can change configurations between transfers by using the &lt;STRONG&gt;SPIx_CTARn&lt;/STRONG&gt; registers. Then from the &lt;STRONG&gt;SPIx_PUSHR&lt;/STRONG&gt; register as stated by Mark you would select the slave to communicate with as well as the CTAR to use with the field SPIx_PUSHR[CTAS]. Refer to SPI chapter in Reference Manual for more details about CTAR registers. If you have further doubts please let us know.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2015 00:53:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357548#M17930</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-03-05T00:53:33Z</dc:date>
    </item>
    <item>
      <title>Re: different chipselect selection for SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357549#M17931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello sir &lt;/P&gt;&lt;P&gt;actually i asked because some controller has register for each chipselect.but there is only one CTAR register.There is&lt;/P&gt;&lt;P&gt;Do not write to the CTAR &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;registers while the module is in the Running state.there for we have to stop spi then change CTAR then restart spi .that option available only for this so is there is any other options.i wrote code for spi that is working.but if am using one spi with different chip select i have to change ctar register .is it required to stop spi and load new one&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2015 08:16:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357549#M17931</guid>
      <dc:creator>lijofrancis</dc:creator>
      <dc:date>2015-03-05T08:16:53Z</dc:date>
    </item>
    <item>
      <title>Re: different chipselect selection for SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357550#M17932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is what I see.&amp;nbsp; In section 3.9.4.3 of the K60 Reference Manual:&lt;/P&gt;&lt;P&gt;This device supports two CTARs on all instances of the SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you have two sets of control-timing you can select between (&lt;STRONG&gt;SPIx_CTAR0 &amp;amp; &lt;STRONG&gt;SPIx_CTAR1) &lt;/STRONG&gt;&lt;/STRONG&gt;for each SPIx_PUSHR operation, which may indeed be 'fewer' than the available CS selections in a SPI instantiation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2015 21:53:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357550#M17932</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2015-03-05T21:53:47Z</dc:date>
    </item>
    <item>
      <title>Re: different chipselect selection for SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357551#M17933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lijo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Earl mentioned, U can make use of 2 SPI configurations using 2 CTARs supported by each SPI module as per the K60 Manual. I think this seems to resolve your issue. Did u get a chance to try it out ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2015 04:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/different-chipselect-selection-for-SPI/m-p/357551#M17933</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2015-03-12T04:22:08Z</dc:date>
    </item>
  </channel>
</rss>