<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KL46 not waking up from VLLS3 mode using rtc alarm</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL46-not-waking-up-from-VLLS3-mode-using-rtc-alarm/m-p/356095#M17772</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would suggest refer AN4857 which is available at;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/rf_if/doc/app_note/AN4857.pdf" title="http://cache.freescale.com/files/rf_if/doc/app_note/AN4857.pdf"&gt;http://cache.freescale.com/files/rf_if/doc/app_note/AN4857.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope it helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Oct 2014 09:11:07 GMT</pubDate>
    <dc:creator>Rick_Li</dc:creator>
    <dc:date>2014-10-29T09:11:07Z</dc:date>
    <item>
      <title>KL46 not waking up from VLLS3 mode using rtc alarm</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL46-not-waking-up-from-VLLS3-mode-using-rtc-alarm/m-p/356094#M17771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I'm trying to wake up the KL46 processor from vlls3 mode using RTC alarm. But it is not waking. Even RTC seconds interrupt is not able to wake up the processor from VLLS3 mode only pin interrupt is working.&lt;/P&gt;&lt;P&gt;Can anyone help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Shabana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Oct 2014 05:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL46-not-waking-up-from-VLLS3-mode-using-rtc-alarm/m-p/356094#M17771</guid>
      <dc:creator>shabana</dc:creator>
      <dc:date>2014-10-28T05:22:14Z</dc:date>
    </item>
    <item>
      <title>Re: KL46 not waking up from VLLS3 mode using rtc alarm</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL46-not-waking-up-from-VLLS3-mode-using-rtc-alarm/m-p/356095#M17772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would suggest refer AN4857 which is available at;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/rf_if/doc/app_note/AN4857.pdf" title="http://cache.freescale.com/files/rf_if/doc/app_note/AN4857.pdf"&gt;http://cache.freescale.com/files/rf_if/doc/app_note/AN4857.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope it helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2014 09:11:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL46-not-waking-up-from-VLLS3-mode-using-rtc-alarm/m-p/356095#M17772</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2014-10-29T09:11:07Z</dc:date>
    </item>
    <item>
      <title>Re: KL46 not waking up from VLLS3 mode using rtc alarm</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL46-not-waking-up-from-VLLS3-mode-using-rtc-alarm/m-p/356096#M17773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shabana,&lt;/P&gt;&lt;P&gt;I was wondering if you can upload your demo to the community, then I can run the demo with FRDM-KL46Z board.&lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Oct 2014 01:55:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL46-not-waking-up-from-VLLS3-mode-using-rtc-alarm/m-p/356096#M17773</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-10-31T01:55:41Z</dc:date>
    </item>
    <item>
      <title>Re: KL46 not waking up from VLLS3 mode using rtc alarm</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL46-not-waking-up-from-VLLS3-mode-using-rtc-alarm/m-p/356097#M17774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shabana-san,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess the RTC was not clocked in the power mode. By default, RTC is clocked by OSC32KCLK which would be stopped in the power mode. I think you had better change the setting of SIM_SOPT1[OSC32KSEL] from OSC32KCLK to LPO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Yasuhiko Koumoto.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Nov 2014 12:36:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL46-not-waking-up-from-VLLS3-mode-using-rtc-alarm/m-p/356097#M17774</guid>
      <dc:creator>yasuhikokoumoto</dc:creator>
      <dc:date>2014-11-02T12:36:13Z</dc:date>
    </item>
  </channel>
</rss>