<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Interrupts with KDS</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupts-with-KDS/m-p/355824#M17749</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello John:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may refer to the following thread about the same question:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/458130"&gt;Re: setup interrupts KDS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Dec 2014 23:03:00 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2014-12-16T23:03:00Z</dc:date>
    <item>
      <title>Interrupts with KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupts-with-KDS/m-p/355823#M17748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am moving some code from an MK20 part (written with Code Warrior 10.6) to the MK22FN512 and using KDS.&amp;nbsp; Apparently KDS handles interrupts differently than CW and I am having trouble.&amp;nbsp; KDS does not give me access to the NVICICPR and NVICISER registers.&amp;nbsp; I need to know how to 1) enable an interrupt in the NVIC and 2) to point the interrupt vector to my interrupt routine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help?&amp;nbsp; Sorry for such a simple question, but I'd rather just translate these two tiny bits of code and be on my way rather than spend a week figuring out processor expert or digging through the overwhelming documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2014 20:23:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupts-with-KDS/m-p/355823#M17748</guid>
      <dc:creator>JohnMusselman</dc:creator>
      <dc:date>2014-12-16T20:23:00Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupts with KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupts-with-KDS/m-p/355824#M17749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello John:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may refer to the following thread about the same question:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/458130"&gt;Re: setup interrupts KDS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2014 23:03:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupts-with-KDS/m-p/355824#M17749</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-12-16T23:03:00Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupts with KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupts-with-KDS/m-p/355825#M17750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp; Yes, with KDS the definition of the NVIC registers has changed.&amp;nbsp; NVICISER1 is now NVIC--&amp;gt;ISER[1], for example.&amp;nbsp; The proper files are already included in the project.&amp;nbsp; I'm still trying to get the board to work so can't verify that this and the interrupt vector actually work, but it does build now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2014 20:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupts-with-KDS/m-p/355825#M17750</guid>
      <dc:creator>JohnMusselman</dc:creator>
      <dc:date>2014-12-17T20:42:04Z</dc:date>
    </item>
  </channel>
</rss>