<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 P.E. K70 Clock setup. MCG External Osc selection</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181587#M1772</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why is system osc 0 the only external clock available in the MCG clk source settings? From the diagram in figure 5.1 it appears I should be able to select osc 1 as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Jul 2012 08:33:05 GMT</pubDate>
    <dc:creator>crezyoz</dc:creator>
    <dc:date>2012-07-21T08:33:05Z</dc:date>
    <item>
      <title>P.E. K70 Clock setup. MCG External Osc selection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181587#M1772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why is system osc 0 the only external clock available in the MCG clk source settings? From the diagram in figure 5.1 it appears I should be able to select osc 1 as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jul 2012 08:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181587#M1772</guid>
      <dc:creator>crezyoz</dc:creator>
      <dc:date>2012-07-21T08:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: P.E. K70 Clock setup. MCG External Osc selection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181588#M1773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Phil! We are working on it! As soon as possible we will answer you.&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2012 17:25:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181588#M1773</guid>
      <dc:creator>squadmcu</dc:creator>
      <dc:date>2012-10-26T17:25:58Z</dc:date>
    </item>
    <item>
      <title>Re: P.E. K70 Clock setup. MCG External Osc selection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181589#M1774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. It seems I should be able to use OSC1 as well but from what I understand it requires multiple clock modes to be switched through in order to get it to work. ? I am uneasy about that so I have temporarily hacked an external OSC on my board to use OSC0. I look forward to your help with this. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Oct 2012 14:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181589#M1774</guid>
      <dc:creator>crezyoz</dc:creator>
      <dc:date>2012-10-27T14:47:29Z</dc:date>
    </item>
    <item>
      <title>Re: P.E. K70 Clock setup. MCG External Osc selection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181590#M1775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Does Freescale have FORMAL release sample code for this issue? I have the same problem ? &lt;/P&gt;&lt;P&gt;&amp;nbsp; I use CW 10.5 and K70 &amp;amp; KINETIS_120MHZ_SC!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2014 02:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181590#M1775</guid>
      <dc:creator>applefly</dc:creator>
      <dc:date>2014-04-02T02:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: P.E. K70 Clock setup. MCG External Osc selection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181591#M1776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the problem you have?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is about the missing OSC1 option in processor expert, there is an explanation for that. Please check my pair of inputs at the next thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/389169#389169" title="https://community.freescale.com/message/389169#389169"&gt;https://community.freescale.com/message/389169#389169&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you have a different issue, I suggest you to create a new thread with the description so it is more visible to the community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2014 05:03:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/P-E-K70-Clock-setup-MCG-External-Osc-selection/m-p/181591#M1776</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-04-02T05:03:26Z</dc:date>
    </item>
  </channel>
</rss>