<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: External crystal TRK-KEA128 Demo Board</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354807#M17650</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello jeremyzhou,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;your example is not working... You have to initialize the OSC_CR register with 0xB6 and not 0xA6...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I wanted to have a processor expert projekt. Unfortunately there is a processor expert bug in the CPU_Init.c in Kinetis Sudio 1.1 and CW MCU (Eclipse). The OSC_CR register is not initialized in CPU_Init.c line 118 you have to add CPU_OSC_CR_CONFIG_0. The bug is fixed in Kinetis Studio 2 without notice...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Mar 2015 08:29:14 GMT</pubDate>
    <dc:creator>sebastianprenge</dc:creator>
    <dc:date>2015-03-02T08:29:14Z</dc:date>
    <item>
      <title>External crystal TRK-KEA128 Demo Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354803#M17646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we have a TRK-KEA128 demo board with a PKEAZ128MLK chip. The board has a external crystal (Y2) which is conntected to PIN 13 (EXTAL) and 14 (XTAL). The cyrstal is not in the documentation but physical on the board. Unfortunately the crystal is not working if ICS mode FEE is selected. My project is a minimal Processor Expert Kinetis Dev Studio sample with CPU Bean, 250ms Timer Bean and LED Bean. The LED is toggeled with the timer event. The project is doing fine if ICS mode is FEI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;Seb&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2014 14:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354803#M17646</guid>
      <dc:creator>sebastianprenge</dc:creator>
      <dc:date>2014-12-16T14:31:01Z</dc:date>
    </item>
    <item>
      <title>Re: External crystal TRK-KEA128 Demo Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354804#M17647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian,&lt;/P&gt;&lt;P&gt;I was wondering if you can show the the location of Y2, as I've not found the Y2 you mentioned in the TRK-KEA128 board until now.&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can upload your project, then I can run it with the TRK-KEA128 board.&lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2014 07:42:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354804#M17647</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-12-17T07:42:09Z</dc:date>
    </item>
    <item>
      <title>Re: External crystal TRK-KEA128 Demo Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354805#M17648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I also got the new board rev.D with the Y2 crystal and here, too, it doesn't work. The symptom is that after starting the debugger it just hangs. I also tried to detect any clock directly at the crystal, but there is nothing going on. Did you make any progress on this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Dec 2014 21:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354805#M17648</guid>
      <dc:creator>ChrisN</dc:creator>
      <dc:date>2014-12-21T21:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: Re: External crystal TRK-KEA128 Demo Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354806#M17649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian,&lt;/P&gt;&lt;P&gt;I've attached a demo which runs in FBE mode on TRK-KEA128 REV C, as I didn't have the TRK-KEA128 REV D on hand.&lt;/P&gt;&lt;P&gt;Please refer to it for details.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Dec 2014 09:00:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354806#M17649</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-12-23T09:00:32Z</dc:date>
    </item>
    <item>
      <title>Re: External crystal TRK-KEA128 Demo Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354807#M17650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello jeremyzhou,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;your example is not working... You have to initialize the OSC_CR register with 0xB6 and not 0xA6...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I wanted to have a processor expert projekt. Unfortunately there is a processor expert bug in the CPU_Init.c in Kinetis Sudio 1.1 and CW MCU (Eclipse). The OSC_CR register is not initialized in CPU_Init.c line 118 you have to add CPU_OSC_CR_CONFIG_0. The bug is fixed in Kinetis Studio 2 without notice...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 08:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/External-crystal-TRK-KEA128-Demo-Board/m-p/354807#M17650</guid>
      <dc:creator>sebastianprenge</dc:creator>
      <dc:date>2015-03-02T08:29:14Z</dc:date>
    </item>
  </channel>
</rss>