<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Disable NMI_b pin/interrupt KL04Z?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354183#M17624</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, is the only thing you need to do. Usually in IAR there is a section in the linker called m_flash_config and at some point in your code you should see something similar to this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(In the project I am using now it's inside startup_MK64F12.s). When you find this section you only need to change the bits corresponding to the NMI pin (You can check that in the Reference Manual of the device).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SECTION FlashConfig:CODE&lt;/P&gt;&lt;P&gt;__FlashConfig&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DCD 0xFFFFFFFF&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DCD 0xFFFFFFFF&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DCD 0xFFFFFFFF&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DCD 0xFFFFFFFE&lt;/P&gt;&lt;P&gt;__FlashConfig_End&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Santiago&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Dec 2015 16:36:46 GMT</pubDate>
    <dc:creator>santiago_gonzal</dc:creator>
    <dc:date>2015-12-22T16:36:46Z</dc:date>
    <item>
      <title>Disable NMI_b pin/interrupt KL04Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354179#M17620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I disable NMI Interrupt at startup of μController MKL04Z32VFK4 using CodeWarrior but without Processor Expert? I've seen many threads here in the community regarding my problem and I came to the conclusion that to solve my problem I should disable NMI Interrupt at startup, because I'm using PTB5 as its alternate function of ADC channel through a pull-down network. I've searched the Reference Manual and found that for that I should change the Flash Configurations of the microcontroller that were then loaded at boot to &lt;EM&gt;Flash Option Register (FTFA_FOPT)&lt;/EM&gt;. The problem here is the only examples I came across all involves changing this Flash Configurations through PE interface, my question is how can this be accomplished using just plain code and none of Rapid Application Development features.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for your help. :smileywink:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 15:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354179#M17620</guid>
      <dc:creator>rflmota</dc:creator>
      <dc:date>2015-03-26T15:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: Disable NMI_b pin/interrupt KL04Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354180#M17621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ricardo, I had a similar issue with the KL02. The solution from Freescale is attached. Probably the same or very similar on the KL04 if you research the reference manual. Its all in there but quite hard to find and piece together without an example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John Cottier.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 16:23:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354180#M17621</guid>
      <dc:creator>jcottier</dc:creator>
      <dc:date>2015-03-26T16:23:29Z</dc:date>
    </item>
    <item>
      <title>Re: Disable NMI_b pin/interrupt KL04Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354181#M17622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Many thanks &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jcottier"&gt;jcottier&lt;/A&gt; your tips helped me with solving exactly the problem! :smileywink: &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Apr 2015 10:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354181#M17622</guid>
      <dc:creator>rflmota</dc:creator>
      <dc:date>2015-04-03T10:01:43Z</dc:date>
    </item>
    <item>
      <title>Re: Disable NMI_b pin/interrupt KL04Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354182#M17623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I had the same problem but the solution above didn't work&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use IAR to program and debug, can you advice what is the address of the byte to be changed to FB? Is it the only thing I must do?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MKE04Z8VWJ4 uc&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Thank you in advance for your help&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Dec 2015 06:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354182#M17623</guid>
      <dc:creator>mohamedabdelmag</dc:creator>
      <dc:date>2015-12-20T06:54:42Z</dc:date>
    </item>
    <item>
      <title>Re: Disable NMI_b pin/interrupt KL04Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354183#M17624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, is the only thing you need to do. Usually in IAR there is a section in the linker called m_flash_config and at some point in your code you should see something similar to this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(In the project I am using now it's inside startup_MK64F12.s). When you find this section you only need to change the bits corresponding to the NMI pin (You can check that in the Reference Manual of the device).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SECTION FlashConfig:CODE&lt;/P&gt;&lt;P&gt;__FlashConfig&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DCD 0xFFFFFFFF&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DCD 0xFFFFFFFF&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DCD 0xFFFFFFFF&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DCD 0xFFFFFFFE&lt;/P&gt;&lt;P&gt;__FlashConfig_End&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Santiago&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2015 16:36:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disable-NMI-b-pin-interrupt-KL04Z/m-p/354183#M17624</guid>
      <dc:creator>santiago_gonzal</dc:creator>
      <dc:date>2015-12-22T16:36:46Z</dc:date>
    </item>
  </channel>
</rss>