<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックSD support on FRDM-K22F</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-support-on-FRDM-K22F/m-p/352353#M17466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a plan to support the FAT file system on the SD interface on the FRDM-K22F platform? (This can be either stand-alone or as part of the MQX package.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand the limitation of not having the HD interface (one data line versus four), but I don't need the speed - just a basic interface for logging, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the support is there now and I'm just not looking at the right places, some pointers on the implementation would be great.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 26 Oct 2014 17:22:52 GMT</pubDate>
    <dc:creator>davepfaltzgraff</dc:creator>
    <dc:date>2014-10-26T17:22:52Z</dc:date>
    <item>
      <title>SD support on FRDM-K22F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-support-on-FRDM-K22F/m-p/352353#M17466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a plan to support the FAT file system on the SD interface on the FRDM-K22F platform? (This can be either stand-alone or as part of the MQX package.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand the limitation of not having the HD interface (one data line versus four), but I don't need the speed - just a basic interface for logging, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the support is there now and I'm just not looking at the right places, some pointers on the implementation would be great.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 26 Oct 2014 17:22:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-support-on-FRDM-K22F/m-p/352353#M17466</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2014-10-26T17:22:52Z</dc:date>
    </item>
    <item>
      <title>Re: SD support on FRDM-K22F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-support-on-FRDM-K22F/m-p/352354#M17467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;I've not found the demo that integrated with filesystem so far and I'll contact with KSDK team to confirm it later.&lt;/P&gt;&lt;P&gt;However I'd like to recommend two practical experiments about SD and I think they're worth to refer to.&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/07/30/fatfs-with-kinetis/" title="http://mcuoneclipse.com/2012/07/30/fatfs-with-kinetis/"&gt;FatFs with Kinetis | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2014/07/13/multi-drive-support-with-fatfs/" title="http://mcuoneclipse.com/2014/07/13/multi-drive-support-with-fatfs/"&gt;Multi-Drive Support with FatFS | MCU on Eclipse&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Oct 2014 03:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-support-on-FRDM-K22F/m-p/352354#M17467</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-10-28T03:02:48Z</dc:date>
    </item>
  </channel>
</rss>