<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K20 Resource Manual--PDB Channel n Status Register (PDBx_CHS), CF field in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-Resource-Manual-PDB-Channel-n-Status-Register-PDBx-CHS-CF/m-p/350466#M17270</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see a note that this field has a write 0 to clear.&amp;nbsp;&amp;nbsp; Is this a type, the convention used up to this point in the resource manual is to use write 1 to clear.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Oct 2014 10:30:58 GMT</pubDate>
    <dc:creator>larryhartman</dc:creator>
    <dc:date>2014-10-24T10:30:58Z</dc:date>
    <item>
      <title>K20 Resource Manual--PDB Channel n Status Register (PDBx_CHS), CF field</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-Resource-Manual-PDB-Channel-n-Status-Register-PDBx-CHS-CF/m-p/350466#M17270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see a note that this field has a write 0 to clear.&amp;nbsp;&amp;nbsp; Is this a type, the convention used up to this point in the resource manual is to use write 1 to clear.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2014 10:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-Resource-Manual-PDB-Channel-n-Status-Register-PDBx-CHS-CF/m-p/350466#M17270</guid>
      <dc:creator>larryhartman</dc:creator>
      <dc:date>2014-10-24T10:30:58Z</dc:date>
    </item>
    <item>
      <title>Re: K20 Resource Manual--PDB Channel n Status Register (PDBx_CHS), CF field</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-Resource-Manual-PDB-Channel-n-Status-Register-PDBx-CHS-CF/m-p/350467#M17271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Larry:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is not a typo, you have to write 0 to clear. This applies for both: [CF] and [ERR] bit fields.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 16:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-Resource-Manual-PDB-Channel-n-Status-Register-PDBx-CHS-CF/m-p/350467#M17271</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-11-05T16:25:42Z</dc:date>
    </item>
  </channel>
</rss>