<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM-K64 break in IRQ</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-break-in-IRQ/m-p/349697#M17181</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems that the problem is that GDB is trying to get an infinite stack-backtrace.&lt;/P&gt;&lt;P&gt;The solution is to add this command to the Debugger-&amp;gt;Commands:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; set backtrace limit 20&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ref:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/327560"&gt;KDS debug for K22F120M in interrupt enviroment.&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Nov 2014 08:49:22 GMT</pubDate>
    <dc:creator>oaf</dc:creator>
    <dc:date>2014-11-19T08:49:22Z</dc:date>
    <item>
      <title>FRDM-K64 break in IRQ</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-break-in-IRQ/m-p/349696#M17180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got into a serious problem today when trying to set a breakpoint in an IRQ function on my FRDM-K64 board.&lt;/P&gt;&lt;P&gt;When the breakpoint is hit the console is continuously showing some read from target, it will not stop&lt;/P&gt;&lt;P&gt;and the stack-frame is only partly filled in namely the function-name of the break-point function&lt;/P&gt;&lt;P&gt;is shown but not the previous ones....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The HDTR Debug [GDB SEGGER J-Link Debugging] JLinkGDBServerCL:&lt;/P&gt;&lt;P&gt;Read 4 bytes @ address 0x0000058A (Data = 0xBC08B672)&lt;/P&gt;&lt;P&gt;Read 2 bytes @ address 0x00000584 (Data = 0xB408)&lt;/P&gt;&lt;P&gt;Read 2 bytes @ address 0x00000586 (Data = 0xB662)&lt;/P&gt;&lt;P&gt;Read 2 bytes @ address 0x00000588 (Data = 0x4790)&lt;/P&gt;&lt;P&gt;Read 4 bytes @ address 0x0000058A (Data = 0xBC08B672)&lt;/P&gt;&lt;P&gt;Read 2 bytes @ address 0x00000584 (Data = 0xB408)&lt;/P&gt;&lt;P&gt;Read 2 bytes @ address 0x00000586 (Data = 0xB662)&lt;/P&gt;&lt;P&gt;Read 2 bytes @ address 0x00000588 (Data = 0x4790)&lt;/P&gt;&lt;P&gt;Read 4 bytes @ address 0x0000058A (Data = 0xBC08B672)&lt;/P&gt;&lt;P&gt;Read 2 bytes @ address 0x00000584 (Data = 0xB408)&lt;/P&gt;&lt;P&gt;Read 2 bytes @ address 0x00000586 (Data = 0xB662)&lt;/P&gt;&lt;P&gt;Read 2 bytes @ address 0x00000588 (Data = 0x4790)&lt;/P&gt;&lt;P&gt;Read 4 bytes @ address 0x0000058A (Data = 0xBC08B672)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 11:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-break-in-IRQ/m-p/349696#M17180</guid>
      <dc:creator>oaf</dc:creator>
      <dc:date>2014-11-18T11:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64 break in IRQ</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-break-in-IRQ/m-p/349697#M17181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems that the problem is that GDB is trying to get an infinite stack-backtrace.&lt;/P&gt;&lt;P&gt;The solution is to add this command to the Debugger-&amp;gt;Commands:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; set backtrace limit 20&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ref:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/327560"&gt;KDS debug for K22F120M in interrupt enviroment.&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Nov 2014 08:49:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-break-in-IRQ/m-p/349697#M17181</guid>
      <dc:creator>oaf</dc:creator>
      <dc:date>2014-11-19T08:49:22Z</dc:date>
    </item>
  </channel>
</rss>