<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Wake Up from external pins</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wake-Up-from-external-pins/m-p/349081#M17091</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I wander if the LLWUP unit has to be gated to work. I do&amp;nbsp; not find a bit field to do so. Confirm it does not need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For activating the interrupt of the LLWUP unit from external pin, It is necessary to:&lt;/P&gt;&lt;P&gt;1) enable the interrupt of the pins itself: -&amp;gt; PORT_HAL_SetPinIntMode(BOARD_SW_LLWU_BASE, BOARD_SW_LLWU_PIN, kPortIntFallingEdge);&lt;/P&gt;&lt;P&gt;2) enable the interrupt of the pin in the LLWUP unit -&amp;gt; LLWU_HAL_SetExternalInputPinMode(LLWU_BASE,kLlwuExternalPinDisabled, (llwu_wakeup_pin_t)BOARD_SW_LLWU_EXT_PIN);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are all the previous actions necessary and sufficient???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will the interrupt of the pin change requested or simply ignored in such initialization???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Feb 2015 13:42:34 GMT</pubDate>
    <dc:creator>pietrodicastri</dc:creator>
    <dc:date>2015-02-04T13:42:34Z</dc:date>
    <item>
      <title>Wake Up from external pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wake-Up-from-external-pins/m-p/349081#M17091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I wander if the LLWUP unit has to be gated to work. I do&amp;nbsp; not find a bit field to do so. Confirm it does not need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For activating the interrupt of the LLWUP unit from external pin, It is necessary to:&lt;/P&gt;&lt;P&gt;1) enable the interrupt of the pins itself: -&amp;gt; PORT_HAL_SetPinIntMode(BOARD_SW_LLWU_BASE, BOARD_SW_LLWU_PIN, kPortIntFallingEdge);&lt;/P&gt;&lt;P&gt;2) enable the interrupt of the pin in the LLWUP unit -&amp;gt; LLWU_HAL_SetExternalInputPinMode(LLWU_BASE,kLlwuExternalPinDisabled, (llwu_wakeup_pin_t)BOARD_SW_LLWU_EXT_PIN);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are all the previous actions necessary and sufficient???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will the interrupt of the pin change requested or simply ignored in such initialization???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Feb 2015 13:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wake-Up-from-external-pins/m-p/349081#M17091</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2015-02-04T13:42:34Z</dc:date>
    </item>
    <item>
      <title>Re: Wake Up from external pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wake-Up-from-external-pins/m-p/349082#M17092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See &lt;A href="http://www.utasker.com/kinetis/FRDM-K64F.html" title="http://www.utasker.com/kinetis/FRDM-K64F.html"&gt;http://www.utasker.com/kinetis/FRDM-K64F.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis/LLWU.html" title="http://www.utasker.com/kinetis/LLWU.html"&gt;http://www.utasker.com/kinetis/LLWU.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LLWU has not clock gating. The unit's operation is activated when the processor enters the LLS mode.&lt;/P&gt;&lt;P&gt;You just need to enable the LLWU pin (or LLWU module) plus its interrupt to the NVIC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" target="_blank"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;K64: &lt;A href="http://www.utasker.com/kinetis/FRDM-K64F.html" title="http://www.utasker.com/kinetis/FRDM-K64F.html"&gt;µTasker Kinetis FRDM-K64F support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/TWR-K64F120M.html" title="http://www.utasker.com/kinetis/TWR-K64F120M.html"&gt;µTasker Kinetis TWR-K64F120M support&lt;/A&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Feb 2015 17:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wake-Up-from-external-pins/m-p/349082#M17092</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-02-04T17:23:42Z</dc:date>
    </item>
  </channel>
</rss>