<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックADC Input impedance.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Input-impedance/m-p/347906#M17015</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm a HW designer and is about to design a HW including a KEA64 MCU were we gonna do some ADC readings. &lt;/P&gt;&lt;P&gt;I'm trying to find out the input impedance for the ADC but cannot find this data in the data sheets for KEA64. The only thing if find is Hi-Z state but not what Hi-Z is.&lt;/P&gt;&lt;P&gt;The reasing I'm asking is if were are gonna need to buffer the analog input signal or not. Since this is a cost sensetive&amp;nbsp; project we would like to skip the buffer stage.&lt;/P&gt;&lt;P&gt;And the resolution is not an issue for the input reading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;//Henrik A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Dec 2014 14:49:45 GMT</pubDate>
    <dc:creator>henrikalexander</dc:creator>
    <dc:date>2014-12-12T14:49:45Z</dc:date>
    <item>
      <title>ADC Input impedance.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Input-impedance/m-p/347906#M17015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm a HW designer and is about to design a HW including a KEA64 MCU were we gonna do some ADC readings. &lt;/P&gt;&lt;P&gt;I'm trying to find out the input impedance for the ADC but cannot find this data in the data sheets for KEA64. The only thing if find is Hi-Z state but not what Hi-Z is.&lt;/P&gt;&lt;P&gt;The reasing I'm asking is if were are gonna need to buffer the analog input signal or not. Since this is a cost sensetive&amp;nbsp; project we would like to skip the buffer stage.&lt;/P&gt;&lt;P&gt;And the resolution is not an issue for the input reading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;//Henrik A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Dec 2014 14:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Input-impedance/m-p/347906#M17015</guid>
      <dc:creator>henrikalexander</dc:creator>
      <dc:date>2014-12-12T14:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Input impedance.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Input-impedance/m-p/347907#M17016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Henrik, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I personally measured the resistance of one of the ADC inputs of the KEA02.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The resistance value is about 500 Kohms,&amp;nbsp; and therefore, the ADC input impedance is HIGH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information will be useful for you :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Dec 2014 23:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Input-impedance/m-p/347907#M17016</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2014-12-18T23:49:36Z</dc:date>
    </item>
  </channel>
</rss>