<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K22FN512X Flashloader</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22FN512X-Flashloader/m-p/346003#M16850</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check the pin information in the specific device reference manual. For the K22 you can see the Flash Loader chapter; the image below shows the pin table for the Flashloader:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="k22boot.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49064i2EA6568D816FF0B1/image-size/large?v=v2&amp;amp;px=999" role="button" title="k22boot.jpg" alt="k22boot.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you are using the FRDM-K22F you can use the Virtual COM port connected through the OpenSDA connector that uses theUART1 module: PTE0 and PTE1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information can help you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;Technical Support Engineer&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Mar 2015 18:09:00 GMT</pubDate>
    <dc:creator>adriancano</dc:creator>
    <dc:date>2015-03-24T18:09:00Z</dc:date>
    <item>
      <title>K22FN512X Flashloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22FN512X-Flashloader/m-p/346002#M16849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like programming the microcontroller MK22FN512VLH12 in flashloader method (With FSL_Kinetis_Bootloader_1_1_0).&lt;/P&gt;&lt;P&gt;What are the pins to be connected to the computer?&lt;/P&gt;&lt;P&gt;thank .&lt;/P&gt;&lt;P&gt;Antoine&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 16:26:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22FN512X-Flashloader/m-p/346002#M16849</guid>
      <dc:creator>antoinee</dc:creator>
      <dc:date>2015-03-24T16:26:33Z</dc:date>
    </item>
    <item>
      <title>Re: K22FN512X Flashloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22FN512X-Flashloader/m-p/346003#M16850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check the pin information in the specific device reference manual. For the K22 you can see the Flash Loader chapter; the image below shows the pin table for the Flashloader:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="k22boot.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49064i2EA6568D816FF0B1/image-size/large?v=v2&amp;amp;px=999" role="button" title="k22boot.jpg" alt="k22boot.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you are using the FRDM-K22F you can use the Virtual COM port connected through the OpenSDA connector that uses theUART1 module: PTE0 and PTE1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information can help you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;Technical Support Engineer&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 18:09:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22FN512X-Flashloader/m-p/346003#M16850</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2015-03-24T18:09:00Z</dc:date>
    </item>
    <item>
      <title>Re: K22FN512X Flashloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22FN512X-Flashloader/m-p/346004#M16851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank.:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 13:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22FN512X-Flashloader/m-p/346004#M16851</guid>
      <dc:creator>antoinee</dc:creator>
      <dc:date>2015-03-26T13:59:42Z</dc:date>
    </item>
  </channel>
</rss>