<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Copy flash from one chip to another using JTAG</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Copy-flash-from-one-chip-to-another-using-JTAG/m-p/345202#M16800</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've written some code for the K20 chip, and I'm wondering if it's safe to use a JTAG programmer to copy that code from one chip to another.&amp;nbsp; Is there anything in memory that's perhaps read-only or reserved that could cause problems when dumping the entire memory from one K20 to another?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marlon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Oct 2014 22:10:08 GMT</pubDate>
    <dc:creator>marlonsmith</dc:creator>
    <dc:date>2014-10-22T22:10:08Z</dc:date>
    <item>
      <title>Copy flash from one chip to another using JTAG</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Copy-flash-from-one-chip-to-another-using-JTAG/m-p/345202#M16800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've written some code for the K20 chip, and I'm wondering if it's safe to use a JTAG programmer to copy that code from one chip to another.&amp;nbsp; Is there anything in memory that's perhaps read-only or reserved that could cause problems when dumping the entire memory from one K20 to another?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marlon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 22:10:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Copy-flash-from-one-chip-to-another-using-JTAG/m-p/345202#M16800</guid>
      <dc:creator>marlonsmith</dc:creator>
      <dc:date>2014-10-22T22:10:08Z</dc:date>
    </item>
    <item>
      <title>Re: Copy flash from one chip to another using JTAG</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Copy-flash-from-one-chip-to-another-using-JTAG/m-p/345203#M16801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This really depends the JTAG programmer. As normal, if programmer support this function, it should be safe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Oct 2014 02:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Copy-flash-from-one-chip-to-another-using-JTAG/m-p/345203#M16801</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-10-23T02:34:56Z</dc:date>
    </item>
  </channel>
</rss>