<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Where is the comparator input?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-the-comparator-input/m-p/344578#M16762</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read on the Figure 36-1 of the RM for the K60 the two comparator's input selectable through VRSEL are Vin1 and Vin2. &lt;/P&gt;&lt;P&gt;In my understanding should be somewhere in the pinout of the uC. I don't find.&lt;/P&gt;&lt;P&gt;Maybe there is a good reason why are not there....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Sep 2014 08:00:41 GMT</pubDate>
    <dc:creator>pietrodicastri</dc:creator>
    <dc:date>2014-09-25T08:00:41Z</dc:date>
    <item>
      <title>Where is the comparator input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-the-comparator-input/m-p/344578#M16762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read on the Figure 36-1 of the RM for the K60 the two comparator's input selectable through VRSEL are Vin1 and Vin2. &lt;/P&gt;&lt;P&gt;In my understanding should be somewhere in the pinout of the uC. I don't find.&lt;/P&gt;&lt;P&gt;Maybe there is a good reason why are not there....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 08:00:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-the-comparator-input/m-p/344578#M16762</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2014-09-25T08:00:41Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the comparator input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-the-comparator-input/m-p/344579#M16763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pietro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is more info regarding Vin1 and Vin2 in Chapter 3, please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46260iFCB84B1808F42ABA/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 06:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-the-comparator-input/m-p/344579#M16763</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-09-26T06:35:23Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the comparator input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-the-comparator-input/m-p/344580#M16764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 16:01:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-the-comparator-input/m-p/344580#M16764</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2014-09-26T16:01:19Z</dc:date>
    </item>
  </channel>
</rss>