<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: What and How the SS functionality?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344547#M16759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You..&lt;/P&gt;&lt;P&gt;Now this aspect is clear.&lt;/P&gt;&lt;P&gt;I would need an additional answer if it is possible for You. Please.&lt;/P&gt;&lt;P&gt;Is this SS signal mandatory? In your answer I read the pin is valid.&lt;/P&gt;&lt;P&gt;So no way to work without the SS??&lt;/P&gt;&lt;P&gt;Another mumble I have is in the naming. I need to know if the SOUT pin is the output&lt;/P&gt;&lt;P&gt;for both master and slave. Same of course for the SIN. From the document it appears yes,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 28 Feb 2015 19:11:18 GMT</pubDate>
    <dc:creator>pietrodicastri</dc:creator>
    <dc:date>2015-02-28T19:11:18Z</dc:date>
    <item>
      <title>What and How the SS functionality?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344545#M16757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I need to find the documentation for using the SS pin in slave mode. &lt;/P&gt;&lt;P&gt;The RM is here and there referring to the SS signal, but&lt;/P&gt;&lt;P&gt;1) I don t see where this pin is, maybe is overlapped with one PCS ????&lt;/P&gt;&lt;P&gt;2) Is it mandatory to use it? Is somewhere written how to select/deselect the usage? &lt;/P&gt;&lt;P&gt;3) If I choice not to use, how to handle the transfer initiated and aborted by a master? (the fraction of data..)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2015 15:45:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344545#M16757</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2015-02-27T15:45:06Z</dc:date>
    </item>
    <item>
      <title>Re: What and How the SS functionality?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344546#M16758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pietro,&lt;/P&gt;&lt;P&gt;The SS is overlapped with the SPIx_PCS0, it's illustrated in the Chapter 10: Signal Multiplexing and Signal Descriptions in the RM and you can find it, the Fig1 shows K60 SS pin allocation.&lt;/P&gt;&lt;P&gt;If you set the SPI interface work in Master mode, the SS pin will be invalid automatically, however when the SPI work in Slave mode, the SS pin will be valid.&lt;/P&gt;&lt;P&gt;Once the Slave mode in MCR[MSTR] is configured, the module is enabled by clearing MCR[HALT] and it should be ensured that module Slave is enabled before enabling it's Master.&lt;/P&gt;&lt;P&gt;After the previous configurations, the Slave modes will initializes successful.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2015-02-28_10-50-17.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50895i91E2196974821FE1/image-size/large?v=v2&amp;amp;px=999" role="button" title="2015-02-28_10-50-17.jpg" alt="2015-02-28_10-50-17.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Fig 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Feb 2015 02:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344546#M16758</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-02-28T02:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: What and How the SS functionality?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344547#M16759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You..&lt;/P&gt;&lt;P&gt;Now this aspect is clear.&lt;/P&gt;&lt;P&gt;I would need an additional answer if it is possible for You. Please.&lt;/P&gt;&lt;P&gt;Is this SS signal mandatory? In your answer I read the pin is valid.&lt;/P&gt;&lt;P&gt;So no way to work without the SS??&lt;/P&gt;&lt;P&gt;Another mumble I have is in the naming. I need to know if the SOUT pin is the output&lt;/P&gt;&lt;P&gt;for both master and slave. Same of course for the SIN. From the document it appears yes,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Feb 2015 19:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344547#M16759</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2015-02-28T19:11:18Z</dc:date>
    </item>
    <item>
      <title>Re: What and How the SS functionality?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344548#M16760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pietro,&lt;/P&gt;&lt;P&gt;If you decide to work in slave mode, the SS pin is only way to active the peripheral chip selection, however this pin need to be asserted manually.&lt;/P&gt;&lt;P&gt;No matter which mode been selected, The SOUT pin will keep output permanently, of course the SIN is same too.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 05:56:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344548#M16760</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-03-02T05:56:43Z</dc:date>
    </item>
    <item>
      <title>Re: What and How the SS functionality?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344549#M16761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 07:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-and-How-the-SS-functionality/m-p/344549#M16761</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2015-03-02T07:47:25Z</dc:date>
    </item>
  </channel>
</rss>