<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KL16 Startup</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-Startup/m-p/344343#M16754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank,&lt;/P&gt;&lt;P&gt;Thank you very much for your focus on Freescale Kinetis product. I'd glad to provide service for you.&lt;/P&gt;&lt;P&gt;Before I give some advice of start the KL16, I think I need clarify the SDK and KDS at first.&lt;/P&gt;&lt;P&gt;SDK is a software development Kit for Kinetis MCU and it's designed to simplify and accelerate application development on Kinetis MCU,&lt;/P&gt;&lt;P&gt;KDS is Kinetis MCU design studio and it's free of charge.&lt;/P&gt;&lt;P&gt;I think it's good way to familiarize yourself with the KL16 through the start with FRDM-KL26 eval board.&lt;/P&gt;&lt;P&gt;So I'd like to suggest that you should download SCH, sample code package, datasheet,etc about the FRDM-KL26 board through the link as follows, it will accelerate you get start with the KL16.&lt;/P&gt;&lt;P&gt;If you have any further questions, please feel free to contact with me.&lt;/P&gt;&lt;P&gt;If you don't have, would you please help to close this SR? Then you'll receive a survey in a moment and please fill it out.&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 28 Feb 2015 04:17:14 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-02-28T04:17:14Z</dc:date>
    <item>
      <title>KL16 Startup</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-Startup/m-p/344342#M16753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just getting started with the KL series using the 32 pin KL16.&amp;nbsp; Simple application, boot, read SPI SEEPROM contents and Xfer to another SPI Device, and go back to sleep.&lt;/P&gt;&lt;P&gt;However, have never used the freescale devices before.&amp;nbsp; So, I am looking for some guidance to get started.&amp;nbsp; I was going to order the Freedom KL26 eval board to familiarize myself with the device and implement a boot loader.&amp;nbsp; In addition, I was going to use the eval board as interface to program my prototypes when I receive 'em.&lt;/P&gt;&lt;P&gt;I see a lot of SDK/IDE's and not sure which is best and or too complicated, some are free and some are not.&amp;nbsp; I want to keep it as simple as possible for a noob like me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Oh before anyone asks, "why am I using the KL16 for such a "simple" application," that is what I was given to work with.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2015 12:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-Startup/m-p/344342#M16753</guid>
      <dc:creator>frankbannon</dc:creator>
      <dc:date>2015-02-27T12:34:14Z</dc:date>
    </item>
    <item>
      <title>Re: KL16 Startup</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-Startup/m-p/344343#M16754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank,&lt;/P&gt;&lt;P&gt;Thank you very much for your focus on Freescale Kinetis product. I'd glad to provide service for you.&lt;/P&gt;&lt;P&gt;Before I give some advice of start the KL16, I think I need clarify the SDK and KDS at first.&lt;/P&gt;&lt;P&gt;SDK is a software development Kit for Kinetis MCU and it's designed to simplify and accelerate application development on Kinetis MCU,&lt;/P&gt;&lt;P&gt;KDS is Kinetis MCU design studio and it's free of charge.&lt;/P&gt;&lt;P&gt;I think it's good way to familiarize yourself with the KL16 through the start with FRDM-KL26 eval board.&lt;/P&gt;&lt;P&gt;So I'd like to suggest that you should download SCH, sample code package, datasheet,etc about the FRDM-KL26 board through the link as follows, it will accelerate you get start with the KL16.&lt;/P&gt;&lt;P&gt;If you have any further questions, please feel free to contact with me.&lt;/P&gt;&lt;P&gt;If you don't have, would you please help to close this SR? Then you'll receive a survey in a moment and please fill it out.&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Feb 2015 04:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-Startup/m-p/344343#M16754</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-02-28T04:17:14Z</dc:date>
    </item>
  </channel>
</rss>