<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックHello, I am trying to program a KL16 via the Multilink. It worked fine, but then it shows the &amp;quot;Device is secure.Erase to unsecure&amp;quot;. I keep pressing Yes. AFter doing this twice the &amp;quot;Multilink&amp;quot; not connected is shown. There was another board that was doing</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-I-am-trying-to-program-a-KL16-via-the-Multilink-It-worked/m-p/343128#M16639</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to program a KL16 via the Multilink. It worked fine, but then it shows the "Device is secure.Erase to unsecure". I keep pressing Yes. AFter doing this twice the "Multilink" not connected is shown. There was another board that was doing the same. But, its now, surprisingly working,except this 1 board.&lt;/P&gt;&lt;P&gt;I tried the Processor halt utility. Still no luck.Uninstalled/installed PE drivers. No luck.&lt;/P&gt;&lt;P&gt;Also, no where in the code have I modified that register (FTFA_FOPT or any such dangerous registers:)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly give me some suggestions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;YUSUP KHAN&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Feb 2015 05:51:27 GMT</pubDate>
    <dc:creator>yusupkhan</dc:creator>
    <dc:date>2015-02-27T05:51:27Z</dc:date>
    <item>
      <title>Hello, I am trying to program a KL16 via the Multilink. It worked fine, but then it shows the "Device is secure.Erase to unsecure". I keep pressing Yes. AFter doing this twice the "Multilink" not connected is shown. There was another board that was doing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-I-am-trying-to-program-a-KL16-via-the-Multilink-It-worked/m-p/343128#M16639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to program a KL16 via the Multilink. It worked fine, but then it shows the "Device is secure.Erase to unsecure". I keep pressing Yes. AFter doing this twice the "Multilink" not connected is shown. There was another board that was doing the same. But, its now, surprisingly working,except this 1 board.&lt;/P&gt;&lt;P&gt;I tried the Processor halt utility. Still no luck.Uninstalled/installed PE drivers. No luck.&lt;/P&gt;&lt;P&gt;Also, no where in the code have I modified that register (FTFA_FOPT or any such dangerous registers:)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly give me some suggestions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;YUSUP KHAN&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2015 05:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-I-am-trying-to-program-a-KL16-via-the-Multilink-It-worked/m-p/343128#M16639</guid>
      <dc:creator>yusupkhan</dc:creator>
      <dc:date>2015-02-27T05:51:27Z</dc:date>
    </item>
    <item>
      <title>Re: Hello, I am trying to program a KL16 via the Multilink. It worked fine, but then it shows the "Device is secure.Erase to unsecure". I keep pressing Yes. AFter doing this twice the "Multilink" not connected is shown. There was another board that was do</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-I-am-trying-to-program-a-KL16-via-the-Multilink-It-worked/m-p/343129#M16640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yusup Khan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two bits in register FTFA_FSEC (MEEN[5:4]) which enables and disables the mass erase capability of flash memory. Register will load value from address 0x40c when starting up.&lt;/P&gt;&lt;P&gt;So, if you disable the mass erase and secure the chip, then, this chip can not re-program anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are not in such case, then, I would suggest try another Multilink to see if it works!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and you can also try a j-link, please refer to:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/457940"&gt;Unlocking K20&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope it helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Feb 2015 03:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hello-I-am-trying-to-program-a-KL16-via-the-Multilink-It-worked/m-p/343129#M16640</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2015-02-28T03:13:38Z</dc:date>
    </item>
  </channel>
</rss>