<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KDS, Kinetis KE06, Hard Fault when Tx and Rx CAN data in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-Kinetis-KE06-Hard-Fault-when-Tx-and-Rx-CAN-data/m-p/343114#M16637</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;last time when I was dealing with CAN was probably three years ago, and I have never used it on any Kinetis devices. So not sure if I can be of any help for your here :-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Aug 2014 07:50:18 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2014-08-08T07:50:18Z</dc:date>
    <item>
      <title>KDS, Kinetis KE06, Hard Fault when Tx and Rx CAN data</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-Kinetis-KE06-Hard-Fault-when-Tx-and-Rx-CAN-data/m-p/343113#M16636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am developing on a FRDM-KE06 board using KDS and also using PE to generate low level code for a design I am working on. I have the MSCAN module set up to interrupt for CAN Receives, but not Transmits. I currently have the CAN filters set to receive all messages. If I just receive CAN messages everything seems fine. If I add code to periodically Transmit a CAN message then I get a Hard Fault and it looks like the PE generated read of the receive frame is where it is exiting via the hard fault. I don't remember having any such issues when coding on a HCS12 part. I looks to me like the MSCAN hardware is the same for both. Any ideas??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Aug 2014 19:39:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-Kinetis-KE06-Hard-Fault-when-Tx-and-Rx-CAN-data/m-p/343113#M16636</guid>
      <dc:creator>bitjockey</dc:creator>
      <dc:date>2014-08-07T19:39:04Z</dc:date>
    </item>
    <item>
      <title>Re: KDS, Kinetis KE06, Hard Fault when Tx and Rx CAN data</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-Kinetis-KE06-Hard-Fault-when-Tx-and-Rx-CAN-data/m-p/343114#M16637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;last time when I was dealing with CAN was probably three years ago, and I have never used it on any Kinetis devices. So not sure if I can be of any help for your here :-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Aug 2014 07:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-Kinetis-KE06-Hard-Fault-when-Tx-and-Rx-CAN-data/m-p/343114#M16637</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-08-08T07:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: KDS, Kinetis KE06, Hard Fault when Tx and Rx CAN data</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-Kinetis-KE06-Hard-Fault-when-Tx-and-Rx-CAN-data/m-p/343115#M16638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Figured out my issue, in my CAN Rx interrupt the structure pointer passed into CAN1_Read was pointing at the CAN Tx Structure which was caused a fault when CAN1_Read was writing to the structure.....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Aug 2014 13:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-Kinetis-KE06-Hard-Fault-when-Tx-and-Rx-CAN-data/m-p/343115#M16638</guid>
      <dc:creator>bitjockey</dc:creator>
      <dc:date>2014-08-08T13:48:29Z</dc:date>
    </item>
  </channel>
</rss>