<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K65 Max UART Baud Rate</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-Max-UART-Baud-Rate/m-p/342673#M16601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;UART0 and UART1 modules operate from the core/system clock, which provides higher performance level for these modules.&lt;/P&gt;&lt;P&gt;The UART0 and UART1 could support up to 180MHz/16 = 11.25MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPUART baud rate = (ASYNCH module clock)/ (SBR[12:0]x(OSR+1)), the Min. value of (SBR[12:0]x(OSR+1)) is 4. &lt;/P&gt;&lt;P&gt;So in theory, the LPUART baud rate could up to MCGPLLCLK/4 = 180MHz/4 = 45MHz.&lt;/P&gt;&lt;P&gt;While, I don't find any material to support this high speed baud rate for LPUART.&lt;/P&gt;&lt;P&gt;I think LPUART could not work as fast as UART0 and UART1, which used for low power mode mainly.&lt;/P&gt;&lt;P&gt;The LPUART baud rate up to 3.75Mbps sounds reasonable.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Aug 2014 09:15:46 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2014-08-14T09:15:46Z</dc:date>
    <item>
      <title>K65 Max UART Baud Rate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-Max-UART-Baud-Rate/m-p/342672#M16600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Question regarding the max UART baud rate on the K65 is that the input clock needs to be divided by 16, hence the max should be 60MHz (bus clock) / 16 = 3.75MHz.  Can anyone confirm this?&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;The K65 LPUART seems to remove the required divide by 16, but I assume that is to allow for the over-sampling feature.  What is the max baud rate on the LPUART?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Aug 2014 14:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-Max-UART-Baud-Rate/m-p/342672#M16600</guid>
      <dc:creator>michaelsteffenf</dc:creator>
      <dc:date>2014-08-07T14:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: K65 Max UART Baud Rate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-Max-UART-Baud-Rate/m-p/342673#M16601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;UART0 and UART1 modules operate from the core/system clock, which provides higher performance level for these modules.&lt;/P&gt;&lt;P&gt;The UART0 and UART1 could support up to 180MHz/16 = 11.25MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPUART baud rate = (ASYNCH module clock)/ (SBR[12:0]x(OSR+1)), the Min. value of (SBR[12:0]x(OSR+1)) is 4. &lt;/P&gt;&lt;P&gt;So in theory, the LPUART baud rate could up to MCGPLLCLK/4 = 180MHz/4 = 45MHz.&lt;/P&gt;&lt;P&gt;While, I don't find any material to support this high speed baud rate for LPUART.&lt;/P&gt;&lt;P&gt;I think LPUART could not work as fast as UART0 and UART1, which used for low power mode mainly.&lt;/P&gt;&lt;P&gt;The LPUART baud rate up to 3.75Mbps sounds reasonable.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Aug 2014 09:15:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-Max-UART-Baud-Rate/m-p/342673#M16601</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-08-14T09:15:46Z</dc:date>
    </item>
  </channel>
</rss>