<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K10 using I2S MIC.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-using-I2S-MIC/m-p/342039#M16556</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a K10P144M120 design. I have a I2S MIC connected to I2S1_RXD0, I2S1_BCLK and I2S1_RX_FS. Can I configure the SAI module for receive only? Do I have to configure the transmit?&amp;nbsp; It appears that the RX BCLK source is from the transmit BCLK. Can I configure the transmit but do not configure the I/O pins?&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Oct 2014 00:08:04 GMT</pubDate>
    <dc:creator>c393</dc:creator>
    <dc:date>2014-10-22T00:08:04Z</dc:date>
    <item>
      <title>K10 using I2S MIC.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-using-I2S-MIC/m-p/342039#M16556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a K10P144M120 design. I have a I2S MIC connected to I2S1_RXD0, I2S1_BCLK and I2S1_RX_FS. Can I configure the SAI module for receive only? Do I have to configure the transmit?&amp;nbsp; It appears that the RX BCLK source is from the transmit BCLK. Can I configure the transmit but do not configure the I/O pins?&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 00:08:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-using-I2S-MIC/m-p/342039#M16556</guid>
      <dc:creator>c393</dc:creator>
      <dc:date>2014-10-22T00:08:04Z</dc:date>
    </item>
    <item>
      <title>Re: K10 using I2S MIC.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-using-I2S-MIC/m-p/342040#M16557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dennis&lt;/P&gt;&lt;P&gt;Yes, you can configure it as receiver only. For your last question, I cannot understand it clearly. Would you please to make me clear? Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Oct 2014 03:21:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-using-I2S-MIC/m-p/342040#M16557</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-10-23T03:21:46Z</dc:date>
    </item>
  </channel>
</rss>