<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: In USB USBRST bit is not getting set.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341059#M16426</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Actually now Im trying using processor expert. In same USB atack there are some example project for MSD using processor expert. In that I have changed the code created in KL25 for KL46.&lt;/P&gt;&lt;P&gt;In UART Im getting following error message..&lt;/P&gt;&lt;P&gt;Waiting for USB mass storage to be attached...&lt;/P&gt;&lt;P&gt;Mass Storage Device Attached&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;================ START OF A NEW SESSION ================&lt;/P&gt;&lt;P&gt;Testing: GET MAX LUN Command..........................OK&lt;/P&gt;&lt;P&gt;Testing: TEST UNIT READY Command...Unsupported(bStatus=0xfffffff9)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: INQUIRY CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: READ CAPACITY CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: READ FORMAT CAPACITIES CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: MODE SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: PREVENT-ALLOW MEDIUM REMOVAL CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: VERIFY CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: WRITE(10) CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: READ(10) CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: START-STOP UNIT CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Test done!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;all the test has been failed..:smileysad:&lt;/P&gt;&lt;P&gt;help me!!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shabana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Sep 2014 10:27:28 GMT</pubDate>
    <dc:creator>shabana</dc:creator>
    <dc:date>2014-09-25T10:27:28Z</dc:date>
    <item>
      <title>In USB USBRST bit is not getting set.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341056#M16423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The following are the things that I have done.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. Im using the Freescale USB stack v4.1.1. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2. The example project that Im refering is msd_msf_generic -&amp;gt; K40.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3. Im converting the K40 project to KL46.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4. In not using the same workspace to create the project instead I have copied the files to some other workspace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is if I connect the USB memory stick the control comes to the ISR but the USBRST bit is not set.&lt;/P&gt;&lt;P&gt;The register looks like the attached picture.&lt;/P&gt;&lt;P&gt;can any one help me!!!!!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shabana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 07:55:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341056#M16423</guid>
      <dc:creator>shabana</dc:creator>
      <dc:date>2014-09-24T07:55:23Z</dc:date>
    </item>
    <item>
      <title>Re: In USB USBRST bit is not getting set.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341057#M16424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shabana m,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I know, there is some code issue in the demo of msd_mfs_generic host from usb stack ver 4.1.1, please kindly refer to &lt;A href="https://community.nxp.com/docs/DOC-101861"&gt;[USB stack ver 4.1.1] a code issue in msd_mfs_generic host demo&lt;/A&gt; for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 10:01:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341057#M16424</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-09-24T10:01:31Z</dc:date>
    </item>
    <item>
      <title>Re: In USB USBRST bit is not getting set.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341058#M16425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan,&lt;/P&gt;&lt;P&gt;The code has been changed as they have said in the link even though the problem is not solved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;shabana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 11:12:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341058#M16425</guid>
      <dc:creator>shabana</dc:creator>
      <dc:date>2014-09-24T11:12:48Z</dc:date>
    </item>
    <item>
      <title>Re: In USB USBRST bit is not getting set.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341059#M16426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Actually now Im trying using processor expert. In same USB atack there are some example project for MSD using processor expert. In that I have changed the code created in KL25 for KL46.&lt;/P&gt;&lt;P&gt;In UART Im getting following error message..&lt;/P&gt;&lt;P&gt;Waiting for USB mass storage to be attached...&lt;/P&gt;&lt;P&gt;Mass Storage Device Attached&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;================ START OF A NEW SESSION ================&lt;/P&gt;&lt;P&gt;Testing: GET MAX LUN Command..........................OK&lt;/P&gt;&lt;P&gt;Testing: TEST UNIT READY Command...Unsupported(bStatus=0xfffffff9)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: INQUIRY CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: READ CAPACITY CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: READ FORMAT CAPACITIES CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: MODE SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: PREVENT-ALLOW MEDIUM REMOVAL CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: VERIFY CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: WRITE(10) CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: REQUEST SENSE CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: READ(10) CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;Testing: START-STOP UNIT CommandFAILED(ff)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Test done!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;all the test has been failed..:smileysad:&lt;/P&gt;&lt;P&gt;help me!!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shabana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2014 10:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341059#M16426</guid>
      <dc:creator>shabana</dc:creator>
      <dc:date>2014-09-25T10:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: In USB USBRST bit is not getting set.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341060#M16427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shabana,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that might be some incompatible issue between the usb stack and the pen driver, just like what is mentioned in the release note for usb stack ver 4.1.1.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46261iFCD583B031354912/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 02:32:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/In-USB-USBRST-bit-is-not-getting-set/m-p/341060#M16427</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-09-26T02:32:29Z</dc:date>
    </item>
  </channel>
</rss>