<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 10Mbps with LAN8720 and K70 - Communication with 10Mbps does not work in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340882#M16382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We work with a proprietary board with CPU K70F120M, PHY LAN8720A, MQX 4.1.1 and Keil uVision MDK Kinetis CortexM 5.12&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Communication with 100Mbps on a 100Mbps-switch works correctly. The green Link-LED is ON. ping is answered. ftp commands are acknowledged.&lt;/P&gt;&lt;P&gt;The MQX functions ENET_get_speed (ehandle); reports correctly "100" Mbps.&lt;/P&gt;&lt;P&gt;ENET_link_status (ehandle); reports "link active".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we connect a 10Mbps-hub in between, the green link-LED is OFF. ping is not answered by the controller. ftp commands are not acknowledged.&lt;/P&gt;&lt;P&gt;The MQX functions ENET_get_speed (ehandle); reports correctly "10" Mbps.&lt;/P&gt;&lt;P&gt;ENET_link_status (ehandle); reports "link active".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The automatic detection of 10 or 100 Mbps seem to be correctly. But no communication is possible&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is to do, to go 10 or 100 Mbps automatically?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Klaus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Mar 2015 13:52:18 GMT</pubDate>
    <dc:creator>klausconzelmann</dc:creator>
    <dc:date>2015-03-23T13:52:18Z</dc:date>
    <item>
      <title>10Mbps with LAN8720 and K70 - Communication with 10Mbps does not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340882#M16382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We work with a proprietary board with CPU K70F120M, PHY LAN8720A, MQX 4.1.1 and Keil uVision MDK Kinetis CortexM 5.12&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Communication with 100Mbps on a 100Mbps-switch works correctly. The green Link-LED is ON. ping is answered. ftp commands are acknowledged.&lt;/P&gt;&lt;P&gt;The MQX functions ENET_get_speed (ehandle); reports correctly "100" Mbps.&lt;/P&gt;&lt;P&gt;ENET_link_status (ehandle); reports "link active".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we connect a 10Mbps-hub in between, the green link-LED is OFF. ping is not answered by the controller. ftp commands are not acknowledged.&lt;/P&gt;&lt;P&gt;The MQX functions ENET_get_speed (ehandle); reports correctly "10" Mbps.&lt;/P&gt;&lt;P&gt;ENET_link_status (ehandle); reports "link active".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The automatic detection of 10 or 100 Mbps seem to be correctly. But no communication is possible&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is to do, to go 10 or 100 Mbps automatically?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Klaus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 13:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340882#M16382</guid>
      <dc:creator>klausconzelmann</dc:creator>
      <dc:date>2015-03-23T13:52:18Z</dc:date>
    </item>
    <item>
      <title>Re: 10Mbps with LAN8720 and K70 - Communication with 10Mbps does not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340883#M16383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Klaus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using RMII mode it is important that the EMAC is set according to the link state (speed and duplex). Therefore ensure that your code is handling the PHY's link state changes accordingly.&lt;/P&gt;&lt;P&gt;Moving from a 100M switch to 10M hub means that the link state wil be changing speed and also duplex setting. A change in duplex setting requires a restart of the Ethernet controller's buffer decriptor handling (flush old BDs, resynchronise and restart).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;K70: &lt;A href="http://www.utasker.com/kinetis/TWR-K70F120M.html" title="http://www.utasker.com/kinetis/TWR-K70F120M.html"&gt;µTasker Kinetis TWR-K70F120M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market &lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2015 19:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340883#M16383</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-03-23T19:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: 10Mbps with LAN8720 and K70 - Communication with 10Mbps does not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340884#M16384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Thank you for your reply.&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;OK so far&lt;/SPAN&gt;. &lt;SPAN class="hps"&gt;RMII&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;is active.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class="hps"&gt;In the function&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;MACNET_initialize&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;()&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;macnet_init.c&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a fixed&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;definition&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;speed&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and duplex to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;10&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;or 100 Mbps&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and full&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;or&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;half duplex&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;occurs&lt;/SPAN&gt;.&lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Where is in MQX 4.1.1 the function Auto Negotiate from us will activated, so speed and duplex are automatically detected and adjusted?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class="hps"&gt;How does the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;continuous&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;detection&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;link state changes&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;MQX&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;4.1.1 and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;reinitialization&lt;/SPAN&gt;?&lt;BR /&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;Or is&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;auto&lt;/SPAN&gt;&lt;SPAN&gt;-negotiate&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;link status&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;detection in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;MQX&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;4.1.1&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;not realized&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and must be added&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;yourself?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Thanks and Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Klaus&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2015 08:56:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340884#M16384</guid>
      <dc:creator>klausconzelmann</dc:creator>
      <dc:date>2015-03-25T08:56:42Z</dc:date>
    </item>
    <item>
      <title>Re: 10Mbps with LAN8720 and K70 - Communication with 10Mbps does not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340885#M16385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Klaus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it may be related to missing functionality in MQX I would use the forum at: &lt;A href="https://community.nxp.com/space/2023"&gt;MQX Software Solutions&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" target="_blank"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;K70: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/TWR-K70F120M.html" target="_blank"&gt;µTasker Kinetis TWR-K70F120M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2015 10:01:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340885#M16385</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-03-25T10:01:02Z</dc:date>
    </item>
    <item>
      <title>Re: 10Mbps with LAN8720 and K70 - Communication with 10Mbps does not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340886#M16386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Hi Mark,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Thank you for your reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class="hps"&gt;I understand that&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;so&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;so&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;that no&lt;/SPAN&gt; &lt;SPAN class="atn hps"&gt;auto-&lt;/SPAN&gt;negotiate &lt;SPAN class="hps"&gt;and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;link status&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;detection in&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;MQX&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;4.1.1&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;are implemented&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;we need to integrate&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;this yourself&lt;/SPAN&gt;.&lt;BR /&gt;&lt;SPAN class="hps"&gt;Thanks for the advice&lt;/SPAN&gt;. &lt;SPAN class="hps"&gt;I'll look&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;in the forum.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class="hps"&gt;Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Klaus&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 06:36:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340886#M16386</guid>
      <dc:creator>klausconzelmann</dc:creator>
      <dc:date>2015-03-26T06:36:08Z</dc:date>
    </item>
    <item>
      <title>Re: 10Mbps with LAN8720 and K70 - Communication with 10Mbps does not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340887#M16387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;About 10Mbit/100Mbit autonegotiation)&lt;/P&gt;&lt;P&gt;For proper work Ethernet module and phy have to work with the same speed/duplex settings.&lt;/P&gt;&lt;P&gt;Problem is that some of PHYs don’t have any wire or any other way how phy could directly inform MCU about changed parameters.&lt;/P&gt;&lt;P&gt;Only way is that MCU use MDC/MDIO communication for reading phy status. Unfortunately this reading is executed during Ethernet mode initialization only in case of MII interface. RMII use default setting is 100Mbit, full duplex.10Mbit speed is now used only in rare cases when very old infrastructure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, basic ways how to add support for autonegotiation is adding task with periodic reads (e.g. once per seccond) of phy status (we will get speed and duplex PHY settings).&lt;/P&gt;&lt;P&gt;Second issue is that kinetis enet module do not offer speed change in runtime for RMII. We have to disable this module (ENET_ECR- ETHEREN=0), set new speed (ENET_RCR-RMII_10T) and enable it again.&lt;/P&gt;&lt;P&gt;On base of new settings from PHY we should call ENET_shutdown() modify speed settings and call ENET_Init() again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 13:07:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/10Mbps-with-LAN8720-and-K70-Communication-with-10Mbps-does-not/m-p/340887#M16387</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-03-26T13:07:23Z</dc:date>
    </item>
  </channel>
</rss>