<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KL17 example</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340860#M16373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Seb&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I never used this with KL17 but if it basically a stripped down version of the KL26 you can also look at&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis/FRDM-KL26Z.html" title="http://www.utasker.com/kinetis/FRDM-KL26Z.html"&gt;http://www.utasker.com/kinetis/FRDM-KL26Z.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This includes every thing that you need (apart for the IIS) and will work out-of-the-box with&lt;/P&gt;&lt;P&gt;CW, KDS, IAR, Keil, Rowley Crossworks, Atollic, CooCox, Green Hills, Standalone GCC or VisualStudio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" target="_blank"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2015 04:02:36 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2015-02-03T04:02:36Z</dc:date>
    <item>
      <title>KL17 example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340857#M16370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm a brand new user of Freescale MCU, and particularly the KL17 family.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a long battery life device using UART, I2C, IIS, SPI, RTC peripherals, and it would be helpfull to find KL17 example projects, which could help me to start working with Kinetis L series MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have already installed the last codewarrior and processor expert version, but I can't find a sample project using a KL17. This is the same issue when I want to build a new processor expert project, I only see KL14/15/16Z MCUs, but no KL17.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for your valuable support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 16:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340857#M16370</guid>
      <dc:creator>marmotte</dc:creator>
      <dc:date>2015-02-02T16:52:40Z</dc:date>
    </item>
    <item>
      <title>Re: KL17 example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340858#M16371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From Q1 2014 on, all new devices (and KL17 is a new one) are only supported in Kinetis Design Studio.&lt;/P&gt;&lt;P&gt;So you need to install Kinetis Design Studio with the Kinetis SDK for the KL17.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 19:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340858#M16371</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-02-02T19:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: KL17 example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340859#M16372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KL17 is using most same modules with KL26,&amp;nbsp; I would recommend to refer KL26 product sample code as a start point.&lt;/P&gt;&lt;P&gt;KL26 sample code based on FRDM-KL26Z could be downloaded from below link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/software/FRDM-KL26Z_SC.exe?fasp=1&amp;amp;WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=exe&amp;amp;WT_ASSET=Downloads&amp;amp;fileExt=.exe" title="http://cache.freescale.com/files/32bit/software/FRDM-KL26Z_SC.exe?fasp=1&amp;amp;WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=exe&amp;amp;WT_ASSET=Downloads&amp;amp;fileExt=.exe"&gt;http://cache.freescale.com/files/32bit/software/FRDM-KL26Z_SC.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 01:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340859#M16372</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-02-03T01:32:46Z</dc:date>
    </item>
    <item>
      <title>Re: KL17 example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340860#M16373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Seb&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I never used this with KL17 but if it basically a stripped down version of the KL26 you can also look at&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis/FRDM-KL26Z.html" title="http://www.utasker.com/kinetis/FRDM-KL26Z.html"&gt;http://www.utasker.com/kinetis/FRDM-KL26Z.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This includes every thing that you need (apart for the IIS) and will work out-of-the-box with&lt;/P&gt;&lt;P&gt;CW, KDS, IAR, Keil, Rowley Crossworks, Atollic, CooCox, Green Hills, Standalone GCC or VisualStudio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" target="_blank"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 04:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340860#M16373</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-02-03T04:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: KL17 example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340861#M16374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your answers, I'll read those documents, and come back to click on the "Correct Answer" button&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 09:44:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-example/m-p/340861#M16374</guid>
      <dc:creator>marmotte</dc:creator>
      <dc:date>2015-02-03T09:44:51Z</dc:date>
    </item>
  </channel>
</rss>