<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: TWR-K70F120M Kit cpu and two UARTs</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-Kit-cpu-and-two-UARTs/m-p/340101#M16343</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, have not been exact enough in description. &lt;BR /&gt;Want to build second application UART port onto a TWR-PROTO board. This second UART is TTL-UART, so do not need RS-232 PHY. TWR is populated with TWR-K70 cpu board, TWR-SER board and TWR-PROTO board. May like to have TWR-LCD too, but can live without it. Can omit TWR-SER, as 'printf' could be catched via USB too.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Need advice, which UART port of cpu board to use (would prefer UART0).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary for TWR-K70F120M cpu board (please tell, if wrong):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; There are 4 possible UART(-Rx-Tx) default pin pairs on TWR-ELEV boards (I call them "twre_UARTx" in contrast to "cpu_UARTx"):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "twre_UART0" is connected to "cpu_UART2"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "twre_UART1" is connected to "cpu_UART3" (if 0 Ohm bridges R134/R135 would be placed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "twer_UART2" is not connected to cpu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "twer_UART3" is not connected to cpu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Prefer using "cpu_UART0". Possible TWR-ELEV pins for "cpu_UART0_RX/TX" are:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTF17/PTF18&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTA1/PTA2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTA15/PTA16&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTB16/PTB17&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTD6/PTD7.&lt;/P&gt;&lt;P&gt;Think that PTF17/PTF18 (secondary connector D53/D54) is best to catch "cpu_UART0_RX/TX" on a TWR-PROTO board.&lt;BR /&gt;Seems to have lowest conflict potential with other TWR boards. Do you agree?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards, Juergen.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2015 07:36:02 GMT</pubDate>
    <dc:creator>jum</dc:creator>
    <dc:date>2015-02-03T07:36:02Z</dc:date>
    <item>
      <title>TWR-K70F120M Kit cpu and two UARTs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-Kit-cpu-and-two-UARTs/m-p/340099#M16341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Plan to use UART with TWR-K70 Kit for application. Would prefer cpu UART0.&lt;BR /&gt;One UART (cpu UART2, cpu SCH signals PTE16/PTE17, ELEV pins A44/A43 via R116/R115) is routed to TWR-SER board and should be used for debug/conio purpose. &lt;BR /&gt;I see one other UART on cpu board tower pins: Cpu UART3, cpu SCH signals PTF8/PTF7, ELEV pins A42/A41 via R135/R134. R135 and R134 have attribut "DNP" (do not place).&lt;/P&gt;&lt;P&gt;1. So to get cpu UART3 Rx/Tx to work: Simply have to place these '0 ohm resistors'/wires ?&lt;/P&gt;&lt;P&gt;2. As PTF8/PTF7 also are connected to 'LCD_D4/LCD_D3': May still use UART3 with active LCD board mounted?&lt;/P&gt;&lt;P&gt;3. See Cpu UART0 (preferred) connected to cpu SCH signals PTF18/PTF17. These are connected to LCD_D14/LCD_D13. Can use them with LCD dismounted?&lt;/P&gt;&lt;P&gt;4. Any other suggestion for second/application UART on this kit?&lt;/P&gt;&lt;P&gt;Best regards, Juergen.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 14:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-Kit-cpu-and-two-UARTs/m-p/340099#M16341</guid>
      <dc:creator>jum</dc:creator>
      <dc:date>2015-02-02T14:53:38Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120M Kit cpu and two UARTs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-Kit-cpu-and-two-UARTs/m-p/340100#M16342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. If customer want to use UART3 at PTF7/PTF8 pins, it need to use TWR-SER2 board instead of TWR-SER board.&lt;/P&gt;&lt;P&gt;2. The PTF7/PTF8 pin with multiple-function, which could affect the LCD display when using both pin for UART communication.&lt;/P&gt;&lt;P&gt;3. Both TWR-SER and TWR-SER2 boards don't provide RS232 PHY connection with PTF17/PTF18 pin, there couldn't use PTF17/PTF18 for UART function.&lt;/P&gt;&lt;P&gt;4. Based on previous analysis, customer could use PTF7/PTF8 of K70 UART3 with TWR-SER2 board with LCD board unmounted.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About TWR-SER2 board info, please check below link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-SER2&amp;amp;lang_cd=en" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-SER2&amp;amp;lang_cd=en"&gt;Enhanced Serial (Dual Ethernet, High-Speed US|Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 03:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-Kit-cpu-and-two-UARTs/m-p/340100#M16342</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-02-03T03:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120M Kit cpu and two UARTs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-Kit-cpu-and-two-UARTs/m-p/340101#M16343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, have not been exact enough in description. &lt;BR /&gt;Want to build second application UART port onto a TWR-PROTO board. This second UART is TTL-UART, so do not need RS-232 PHY. TWR is populated with TWR-K70 cpu board, TWR-SER board and TWR-PROTO board. May like to have TWR-LCD too, but can live without it. Can omit TWR-SER, as 'printf' could be catched via USB too.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Need advice, which UART port of cpu board to use (would prefer UART0).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary for TWR-K70F120M cpu board (please tell, if wrong):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; There are 4 possible UART(-Rx-Tx) default pin pairs on TWR-ELEV boards (I call them "twre_UARTx" in contrast to "cpu_UARTx"):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "twre_UART0" is connected to "cpu_UART2"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "twre_UART1" is connected to "cpu_UART3" (if 0 Ohm bridges R134/R135 would be placed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "twer_UART2" is not connected to cpu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "twer_UART3" is not connected to cpu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Prefer using "cpu_UART0". Possible TWR-ELEV pins for "cpu_UART0_RX/TX" are:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTF17/PTF18&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTA1/PTA2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTA15/PTA16&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTB16/PTB17&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTD6/PTD7.&lt;/P&gt;&lt;P&gt;Think that PTF17/PTF18 (secondary connector D53/D54) is best to catch "cpu_UART0_RX/TX" on a TWR-PROTO board.&lt;BR /&gt;Seems to have lowest conflict potential with other TWR boards. Do you agree?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards, Juergen.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 07:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-Kit-cpu-and-two-UARTs/m-p/340101#M16343</guid>
      <dc:creator>jum</dc:creator>
      <dc:date>2015-02-03T07:36:02Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120M Kit cpu and two UARTs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-Kit-cpu-and-two-UARTs/m-p/340102#M16344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juergen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For K70 product provide Graphic LCD controller, if customer consider to use TWR-LCD-RGB board?&lt;/P&gt;&lt;P&gt;About TWR-LCD-RGB info, please check below link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-LCD-RGB&amp;amp;tid=m32TWR" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-LCD-RGB&amp;amp;tid=m32TWR"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-LCD-RGB&amp;amp;tid=m32TWR&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If using TWR-LDC baord, the PTF17/PTF18 is prefer pins for K70 UART0.&lt;/P&gt;&lt;P&gt;If using TWR-LCD-RGB board, Customer could consider to use PTA14/PTA15 or PTB16/PTB17 or PTD6/PTD7&amp;nbsp; as K70 UART0 pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Feb 2015 08:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-Kit-cpu-and-two-UARTs/m-p/340102#M16344</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-02-04T08:52:41Z</dc:date>
    </item>
  </channel>
</rss>