<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: How to use PGA Kinetis K10 ADC</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PGA-Kinetis-K10-ADC/m-p/339914#M16323</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ERCAN&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Processor Expert Components Library there is a peripheral initialization component named Init_PGA. You can use it to initialize the PGA settings like gain and operating mode. When configuring, just set the Pins/Signals options for Positive and Negative inputs to "Disabled" since the pin initialization is being performed in the ADC_LDD component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Saludos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Oct 2014 16:15:31 GMT</pubDate>
    <dc:creator>santiago_lopez</dc:creator>
    <dc:date>2014-10-22T16:15:31Z</dc:date>
    <item>
      <title>How to use PGA Kinetis K10 ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PGA-Kinetis-K10-ADC/m-p/339913#M16322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I want to use the PGA in Kinetis K10 microcontroller. I try to find Gain option in PE ADC_LDD, but I could not find anything. Is there anyone used PGA from PE. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Okan ERCAN&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 11:14:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PGA-Kinetis-K10-ADC/m-p/339913#M16322</guid>
      <dc:creator>okaner</dc:creator>
      <dc:date>2014-10-21T11:14:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to use PGA Kinetis K10 ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PGA-Kinetis-K10-ADC/m-p/339914#M16323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ERCAN&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Processor Expert Components Library there is a peripheral initialization component named Init_PGA. You can use it to initialize the PGA settings like gain and operating mode. When configuring, just set the Pins/Signals options for Positive and Negative inputs to "Disabled" since the pin initialization is being performed in the ADC_LDD component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Saludos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 16:15:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PGA-Kinetis-K10-ADC/m-p/339914#M16323</guid>
      <dc:creator>santiago_lopez</dc:creator>
      <dc:date>2014-10-22T16:15:31Z</dc:date>
    </item>
    <item>
      <title>Re: How to use PGA Kinetis K10 ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PGA-Kinetis-K10-ADC/m-p/339915#M16324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think that answer was completely right.&amp;nbsp; I didn't get any PGA gain until I DID assign the positive and negative input pins for the PGA.&amp;nbsp; And after that you have to go to the ADC_LDD component and reassign the ADC inputs from the input pins to the PGA outputs PGAxDP and PGAxDM.&amp;nbsp; PEx did not change them automatically. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I implemented this on the TWR-K20D72M board where the microphone is the ADC1_DP0 input and the potentiometer is the ADC1_DM0 input. This allows you to adjust the pot to remove the 0.7V DC bias from the microphone output, which makes a very sensitive audio pickup. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Nov 2014 20:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-PGA-Kinetis-K10-ADC/m-p/339915#M16324</guid>
      <dc:creator>MarkHaines</dc:creator>
      <dc:date>2014-11-02T20:11:41Z</dc:date>
    </item>
  </channel>
</rss>