<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K70 - LCD - max portrait resolution</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCD-max-portrait-resolution/m-p/339434#M16300</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arnaud,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Yes, a 480x800 LCD is possible. In fact during early development of that was the original resolution of the TWR-LCD-RGB, so I can confirm that resolution will definitely work. The 800x600 number is based on bandwidth requirements. The actual max for any one direction is determined by the LCDC_LSR XMAX and YMAX fields. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anthony &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Aug 2014 20:59:29 GMT</pubDate>
    <dc:creator>anthony_huereca</dc:creator>
    <dc:date>2014-08-06T20:59:29Z</dc:date>
    <item>
      <title>K70 - LCD - max portrait resolution</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCD-max-portrait-resolution/m-p/339433#M16299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the maximum resolution for a &lt;STRONG&gt;portrait&lt;/STRONG&gt; TFT driven by a K70 (MK70FN1M0VMJ15) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K70 Sub-Family Reference Manual indicates : Maximum resolution of 800 × 600.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but... the document "Configuring the K70 LCDC Using TWR-LCD-RGB" shows (p.8) an example with a Active frame height of 800.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to interface a portrait LCD 480 x 800, would it be possible ??&lt;/P&gt;&lt;P&gt;LCDC_LSR : XMAX = 480/16 = 30&lt;/P&gt;&lt;P&gt;LCDC_LSR : YMAX = 800&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for any help !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Arnaud&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 16:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCD-max-portrait-resolution/m-p/339433#M16299</guid>
      <dc:creator>arnaud</dc:creator>
      <dc:date>2014-08-06T16:17:45Z</dc:date>
    </item>
    <item>
      <title>Re: K70 - LCD - max portrait resolution</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCD-max-portrait-resolution/m-p/339434#M16300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arnaud,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Yes, a 480x800 LCD is possible. In fact during early development of that was the original resolution of the TWR-LCD-RGB, so I can confirm that resolution will definitely work. The 800x600 number is based on bandwidth requirements. The actual max for any one direction is determined by the LCDC_LSR XMAX and YMAX fields. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anthony &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 20:59:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCD-max-portrait-resolution/m-p/339434#M16300</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2014-08-06T20:59:29Z</dc:date>
    </item>
    <item>
      <title>Re: K70 - LCD - max portrait resolution</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCD-max-portrait-resolution/m-p/339435#M16301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anthony,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Arnaud.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Aug 2014 20:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCD-max-portrait-resolution/m-p/339435#M16301</guid>
      <dc:creator>arnaud</dc:creator>
      <dc:date>2014-08-12T20:50:51Z</dc:date>
    </item>
  </channel>
</rss>