<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Is the MK60FN1M0VLQ12 upper compatible with MK20FN1M0VLQ12?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-MK60FN1M0VLQ12-upper-compatible-with-MK20FN1M0VLQ12/m-p/338755#M16250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Isao&lt;/P&gt;&lt;P&gt;You only can use the PTC3 as a CLKOUT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Sep 2014 17:35:38 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2014-09-24T17:35:38Z</dc:date>
    <item>
      <title>Is the MK60FN1M0VLQ12 upper compatible with MK20FN1M0VLQ12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-MK60FN1M0VLQ12-upper-compatible-with-MK20FN1M0VLQ12/m-p/338753#M16248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the MK60FN1M0VLQ12 if need Ethernet function, otherwise I want to use MK20FN1M0VLQ12.&lt;BR /&gt;Then I was compare the following Signal Multiplexing and Pin Assignments.&lt;BR /&gt;- The 8.2 K20 Signal Multiplexing and Pin Assignments of MK20FN1M0VLQ12 data sheet (K20P144M120SF3 Rev 5)&lt;BR /&gt;- The 8.2 K60 Signal Multiplexing and Pin Assignments of MK60FN1M0VLQ12 data sheet (K60P144M120SF3 Rev 5)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;As a result, the MK60FN1M0VLQ12 is upper compatible with MK20FN1M0VLQ12 except PTA6.&lt;BR /&gt;According to the 8.2 K20 Signal Multiplexing and Pin Assignments, we can assign the PTA6 of the MK20FN1M0VLQ12 as CLKOUT if set PORTA_PCR6[MUX]=5.&lt;BR /&gt;But the MK60FN1M0VLQ12 does not have this feature.&lt;BR /&gt;I cannot find out that how to assign PTA6 as CLKOUT.&lt;BR /&gt;Can we assign the PTA6 of the MK20FN1M0VLQ12 as CLKOUT?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please advise as soon as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Takashima&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Sep 2014 13:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-MK60FN1M0VLQ12-upper-compatible-with-MK20FN1M0VLQ12/m-p/338753#M16248</guid>
      <dc:creator>isaotakashima</dc:creator>
      <dc:date>2014-09-23T13:04:53Z</dc:date>
    </item>
    <item>
      <title>Re: Is the MK60FN1M0VLQ12 upper compatible with MK20FN1M0VLQ12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-MK60FN1M0VLQ12-upper-compatible-with-MK20FN1M0VLQ12/m-p/338754#M16249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Isao,&lt;/P&gt;&lt;P&gt;Please look at following post as I think it will answer your question.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/330775"&gt;Tower BSP/PSP for MK60DX256VMD10 ?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Sep 2014 14:55:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-MK60FN1M0VLQ12-upper-compatible-with-MK20FN1M0VLQ12/m-p/338754#M16249</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2014-09-23T14:55:00Z</dc:date>
    </item>
    <item>
      <title>Re: Is the MK60FN1M0VLQ12 upper compatible with MK20FN1M0VLQ12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-MK60FN1M0VLQ12-upper-compatible-with-MK20FN1M0VLQ12/m-p/338755#M16250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Isao&lt;/P&gt;&lt;P&gt;You only can use the PTC3 as a CLKOUT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 17:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-MK60FN1M0VLQ12-upper-compatible-with-MK20FN1M0VLQ12/m-p/338755#M16250</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2014-09-24T17:35:38Z</dc:date>
    </item>
  </channel>
</rss>