<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Kinetics selection</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetics-selection/m-p/338658#M16245</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Have you checked out the MCU solution advisor? For certain devices it'll even do the pin muxing solving for you &lt;A href="http://freescale.transim.com/solutionadvisor/SolutionAdvisor.aspx?t=features" title="http://freescale.transim.com/solutionadvisor/SolutionAdvisor.aspx?t=features"&gt;http://freescale.transim.com/solutionadvisor/SolutionAdvisor.aspx?t=features&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Mark has good suggestions as well, those should fit your needs well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Aug 2014 21:38:47 GMT</pubDate>
    <dc:creator>anthony_huereca</dc:creator>
    <dc:date>2014-08-06T21:38:47Z</dc:date>
    <item>
      <title>Kinetics selection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetics-selection/m-p/338656#M16243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #222222; font-family: arial, sans-serif;"&gt;I am having trouble selecting the proper Kinetis MCU for &lt;/SPAN&gt;&lt;SPAN style="color: #222222; font-family: arial, sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;evaluation for my new product. I have noticed that the SPI pins &lt;/SPAN&gt;&lt;SPAN style="color: #222222; font-family: arial, sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;are the same as the UART pins. So I need the following &lt;/SPAN&gt;&lt;SPAN style="color: #222222; font-family: arial, sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;connections: 1 or 2 SPI with 7 total CS pins, 2 RS485 UART, &lt;/SPAN&gt;&lt;SPAN style="color: #222222; font-family: arial, sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;USB, DMA, 3.3V, 50+MHz, prefer no BGA package. Application is industrial control.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 16:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetics-selection/m-p/338656#M16243</guid>
      <dc:creator>d2014</dc:creator>
      <dc:date>2014-08-06T16:02:30Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetics selection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetics-selection/m-p/338657#M16244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would start looking at the K20DX256x7 (as on the TWR-K20D72M)&lt;/P&gt;&lt;P&gt;- USB&lt;/P&gt;&lt;P&gt;- 2 SPIs&lt;/P&gt;&lt;P&gt;- 6 UARTs&lt;/P&gt;&lt;P&gt;There are a number of alternative pin mux options for these so you should have no problems finding the combination that you need&lt;/P&gt;&lt;P&gt;- 72MHz&lt;/P&gt;&lt;P&gt;- 100 pin LQFP&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then you could optimise on the package if needed (there are variations with less pins) and possibly on the peripherals (such as the K21 or K22) or choose parts with mort or less FLASH/RAM, max frequency or FPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 21:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetics-selection/m-p/338657#M16244</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-08-06T21:11:28Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetics selection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetics-selection/m-p/338658#M16245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Have you checked out the MCU solution advisor? For certain devices it'll even do the pin muxing solving for you &lt;A href="http://freescale.transim.com/solutionadvisor/SolutionAdvisor.aspx?t=features" title="http://freescale.transim.com/solutionadvisor/SolutionAdvisor.aspx?t=features"&gt;http://freescale.transim.com/solutionadvisor/SolutionAdvisor.aspx?t=features&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Mark has good suggestions as well, those should fit your needs well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 21:38:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetics-selection/m-p/338658#M16245</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2014-08-06T21:38:47Z</dc:date>
    </item>
  </channel>
</rss>