<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Supply Voltage Monitor</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Supply-Voltage-Monitor/m-p/337900#M16154</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Craig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you only want to generate a warning alarm for own supply voltage, my suggestion for you is that you can use LVD (Low voltage detection) function to generate an interrupt. &lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Feb 2015 05:48:57 GMT</pubDate>
    <dc:creator>Paul_Tian</dc:creator>
    <dc:date>2015-02-26T05:48:57Z</dc:date>
    <item>
      <title>Supply Voltage Monitor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Supply-Voltage-Monitor/m-p/337898#M16152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Is the Kinetis K60 able to monitor it's own supply voltage, for instance on an internal analog input?&amp;nbsp; If I want to monitor that voltage do I need to use one of the A/D pins and divide down the voltage?&amp;nbsp; I"m just trying to come up with a simple way to monitor supply (battery) voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Craig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 14:51:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Supply-Voltage-Monitor/m-p/337898#M16152</guid>
      <dc:creator>craigcarder</dc:creator>
      <dc:date>2015-02-25T14:51:28Z</dc:date>
    </item>
    <item>
      <title>Re: Supply Voltage Monitor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Supply-Voltage-Monitor/m-p/337899#M16153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no internal ADC channel that can monitor the power supply. In all my designs I put a voltage divider on each supply that I want to monitor, then connect that to a spare ADC input. If you are sensitive to wasted battery power, you could switch the divider in with a FET or use large value resistors with a bypass capacitor, say 0.1uF or so. In a system that is not limited to using a high impedance divider, it is also practical to connect the same monitor to a comparator input. You can use that comparator function to get an immediate notice when power is going down.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 16:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Supply-Voltage-Monitor/m-p/337899#M16153</guid>
      <dc:creator>gpontis</dc:creator>
      <dc:date>2015-02-25T16:52:12Z</dc:date>
    </item>
    <item>
      <title>Re: Supply Voltage Monitor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Supply-Voltage-Monitor/m-p/337900#M16154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Craig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you only want to generate a warning alarm for own supply voltage, my suggestion for you is that you can use LVD (Low voltage detection) function to generate an interrupt. &lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Feb 2015 05:48:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Supply-Voltage-Monitor/m-p/337900#M16154</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2015-02-26T05:48:57Z</dc:date>
    </item>
  </channel>
</rss>