<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Kinetis L Flash retention lifespan</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-L-Flash-retention-lifespan/m-p/337457#M16096</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ma Hui,&lt;/P&gt;&lt;P&gt;A few related questions:&lt;/P&gt;&lt;P&gt;1) What does "cycling endurance" mean?&amp;nbsp; What happens after 10k cycles?&amp;nbsp; Does the memory cell fail to retain the value?&lt;/P&gt;&lt;P&gt;2) Do reads affect the endurance?&lt;/P&gt;&lt;P&gt;3) Is this spec for a single cell, or does this apply to a sector or block of memory?&amp;nbsp; For example, if the memory is segmented into 1024 bytes does a write to byte 0 and a write to byte 1 count as 1 write in each cell, or 2 writes?&lt;/P&gt;&lt;P&gt;4) Is it reasonable to follow the "curve" and say that after 100k cycles we could expect a minimum of 0.5 years of data retention?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;JT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jan 2015 21:07:23 GMT</pubDate>
    <dc:creator>johntaylor</dc:creator>
    <dc:date>2015-01-13T21:07:23Z</dc:date>
    <item>
      <title>Kinetis L Flash retention lifespan</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-L-Flash-retention-lifespan/m-p/337454#M16093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; My customer seeks confirmation that a user program that has been programmed once (or perhaps twice) into Kinetis KL04 flash will be retained in flash for 10 years.&amp;nbsp; We are not seeking an endurance number (ie....using Flash like EE for many writes)..... just a level of confidence that the original user program in Kinetis KL04 flash will be retained for 10 years.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gordy Carlson&lt;/P&gt;&lt;P&gt;Freescale FAE&lt;/P&gt;&lt;P&gt;Upstate NY&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jan 2015 20:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-L-Flash-retention-lifespan/m-p/337454#M16093</guid>
      <dc:creator>GordyCarlson</dc:creator>
      <dc:date>2015-01-12T20:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis L Flash retention lifespan</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-L-Flash-retention-lifespan/m-p/337455#M16094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gordon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below KL04 Flash specification about reliability is for normal flash operation and retention life:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47921iDC0CA2BBB92CB7A1/image-size/large?v=v2&amp;amp;px=999" title="flash.png" alt="flash.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;For KL04 doesn't have FlexNVM feature, which could bring confusion to customer.&lt;/P&gt;&lt;P&gt;In fact, the NVM here is nonvolatile memory abbreviation, which is no means FlexNVM.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 06:10:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-L-Flash-retention-lifespan/m-p/337455#M16094</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-01-13T06:10:26Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis L Flash retention lifespan</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-L-Flash-retention-lifespan/m-p/337456#M16095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You!&amp;nbsp; Perfect&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Gordy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 16:29:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-L-Flash-retention-lifespan/m-p/337456#M16095</guid>
      <dc:creator>GordyCarlson</dc:creator>
      <dc:date>2015-01-13T16:29:40Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis L Flash retention lifespan</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-L-Flash-retention-lifespan/m-p/337457#M16096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ma Hui,&lt;/P&gt;&lt;P&gt;A few related questions:&lt;/P&gt;&lt;P&gt;1) What does "cycling endurance" mean?&amp;nbsp; What happens after 10k cycles?&amp;nbsp; Does the memory cell fail to retain the value?&lt;/P&gt;&lt;P&gt;2) Do reads affect the endurance?&lt;/P&gt;&lt;P&gt;3) Is this spec for a single cell, or does this apply to a sector or block of memory?&amp;nbsp; For example, if the memory is segmented into 1024 bytes does a write to byte 0 and a write to byte 1 count as 1 write in each cell, or 2 writes?&lt;/P&gt;&lt;P&gt;4) Is it reasonable to follow the "curve" and say that after 100k cycles we could expect a minimum of 0.5 years of data retention?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;JT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 21:07:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-L-Flash-retention-lifespan/m-p/337457#M16096</guid>
      <dc:creator>johntaylor</dc:creator>
      <dc:date>2015-01-13T21:07:23Z</dc:date>
    </item>
  </channel>
</rss>