<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How do i find out the explanation or the definition to the abbreviations for the i/o pins on the kl02 32 pin? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-i-find-out-the-explanation-or-the-definition-to-the/m-p/336876#M16064</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Blaze&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don^t think that there is a general abbreviation list but if you search for tehe one that you are interested in in the user's manual there will be a description of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically all with PTx are GPIOs. PTA1 is Port A bit 1, for example and PTC5 is Port C bit 5, and so on&lt;/P&gt;&lt;P&gt;VREFH and VREFL are the ADC's voltage reference pins (high [highest level reference] and low [lowest level reference])&lt;/P&gt;&lt;P&gt;IRQ is the interrupt function that some pins can be programmed to have.&lt;/P&gt;&lt;P&gt;KBI0_Px is the keyboard interface function that a pin can be programmed to have.&lt;/P&gt;&lt;P&gt;FTMx for FlexTimers&lt;/P&gt;&lt;P&gt;Etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is then a chapter detailing each module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;KE: &lt;A href="http://www.utasker.com/kinetis/FRDM-KE02Z.html" title="http://www.utasker.com/kinetis/FRDM-KE02Z.html"&gt;µTasker FRDM-KE02Z support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/FRDM-KE02Z40M.html" title="http://www.utasker.com/kinetis/FRDM-KE02Z40M.html"&gt;µTasker FRDM-KE02Z40M support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/FRDM-KE06Z.html" title="http://www.utasker.com/kinetis/FRDM-KE06Z.html"&gt;µTasker FRDM-KE06Z support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Mar 2015 03:59:01 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2015-03-21T03:59:01Z</dc:date>
    <item>
      <title>How do i find out the explanation or the definition to the abbreviations for the i/o pins on the kl02 32 pin?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-i-find-out-the-explanation-or-the-definition-to-the/m-p/336875#M16063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do i find out the explanation or the definition to the abbreviations for the i/o pins on the kl02 32 pin mcu? For example some of the ones that are listed are PTB, PTA,IRQ, VREFH, and VREFL. Anything will help, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2015 22:38:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-i-find-out-the-explanation-or-the-definition-to-the/m-p/336875#M16063</guid>
      <dc:creator>blazerogers</dc:creator>
      <dc:date>2015-03-20T22:38:37Z</dc:date>
    </item>
    <item>
      <title>Re: How do i find out the explanation or the definition to the abbreviations for the i/o pins on the kl02 32 pin?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-i-find-out-the-explanation-or-the-definition-to-the/m-p/336876#M16064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Blaze&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don^t think that there is a general abbreviation list but if you search for tehe one that you are interested in in the user's manual there will be a description of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically all with PTx are GPIOs. PTA1 is Port A bit 1, for example and PTC5 is Port C bit 5, and so on&lt;/P&gt;&lt;P&gt;VREFH and VREFL are the ADC's voltage reference pins (high [highest level reference] and low [lowest level reference])&lt;/P&gt;&lt;P&gt;IRQ is the interrupt function that some pins can be programmed to have.&lt;/P&gt;&lt;P&gt;KBI0_Px is the keyboard interface function that a pin can be programmed to have.&lt;/P&gt;&lt;P&gt;FTMx for FlexTimers&lt;/P&gt;&lt;P&gt;Etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is then a chapter detailing each module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;KE: &lt;A href="http://www.utasker.com/kinetis/FRDM-KE02Z.html" title="http://www.utasker.com/kinetis/FRDM-KE02Z.html"&gt;µTasker FRDM-KE02Z support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/FRDM-KE02Z40M.html" title="http://www.utasker.com/kinetis/FRDM-KE02Z40M.html"&gt;µTasker FRDM-KE02Z40M support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/FRDM-KE06Z.html" title="http://www.utasker.com/kinetis/FRDM-KE06Z.html"&gt;µTasker FRDM-KE06Z support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Mar 2015 03:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-i-find-out-the-explanation-or-the-definition-to-the/m-p/336876#M16064</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-03-21T03:59:01Z</dc:date>
    </item>
  </channel>
</rss>