<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Where is _set_clock???? defined?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-set-clock-defined/m-p/336157#M16038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rick Meyer,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which demo you are referring to ? is it &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4800SW.zip" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4800SW.zip"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4800SW.zip&lt;/A&gt; ?&amp;nbsp; Please kindly help to clarify. Thanks for your patience:smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Sep 2014 02:36:29 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2014-09-23T02:36:29Z</dc:date>
    <item>
      <title>Where is _set_clock???? defined?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-set-clock-defined/m-p/336156#M16037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I'm working with the TWR_K60F120M card, and trying to use AN4520 and AN4800 to talk to an I2S device.&lt;/P&gt;&lt;P&gt;Porting most of the code has been pretty straight forward but I'm running into an issue.&lt;/P&gt;&lt;P&gt;Both "_set_clock_112896();" and "_set_clock_122800();" are defined in the function _12s_set_rate(int).&lt;/P&gt;&lt;P&gt;The appnotes do not show the implementation and I am not having any luck locating it in other examples for the tower systems.&lt;/P&gt;&lt;P&gt;I have looked on the Kinetis Header files from the site as well as in the Kinetis_120 bear metal example files.&lt;/P&gt;&lt;P&gt;I did verify that teh "use CMSIS" box is checked in the setup for the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Sep 2014 17:47:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-set-clock-defined/m-p/336156#M16037</guid>
      <dc:creator>rmeyer_arrow</dc:creator>
      <dc:date>2014-09-22T17:47:51Z</dc:date>
    </item>
    <item>
      <title>Re: Where is _set_clock???? defined?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-set-clock-defined/m-p/336157#M16038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rick Meyer,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which demo you are referring to ? is it &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4800SW.zip" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4800SW.zip"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4800SW.zip&lt;/A&gt; ?&amp;nbsp; Please kindly help to clarify. Thanks for your patience:smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Sep 2014 02:36:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-set-clock-defined/m-p/336157#M16038</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-09-23T02:36:29Z</dc:date>
    </item>
    <item>
      <title>Re: Where is _set_clock???? defined?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-set-clock-defined/m-p/336158#M16039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes that is the file.&amp;nbsp; Thank you.&lt;/P&gt;&lt;P&gt;Apparently the search that lead me to the appnote did not have the file attached or referenced.&lt;/P&gt;&lt;P&gt;Since the first appnote did not have any SW files I assumed this one did not as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the prompt answer.&lt;/P&gt;&lt;P&gt;Have a great day.&lt;/P&gt;&lt;P&gt;Rick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Sep 2014 14:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-is-set-clock-defined/m-p/336158#M16039</guid>
      <dc:creator>rmeyer_arrow</dc:creator>
      <dc:date>2014-09-23T14:52:18Z</dc:date>
    </item>
  </channel>
</rss>