<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: ISR code not working</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336138#M16029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Vinod,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question, I have not the FRDM-KL04 board on hand, but I have FRDM-KL02Z board, I have tested the code on my FRDM-KL02Z board, I found out that the LPTMR0_PSR[PCS]=11 in binary for unknown reason&amp;nbsp; in default state, in the case, it selects the OSCERCLK as clock source, in the case, you should set the OSC32KSEL in SIM_SOPT1 as 10 in binary, in the setting, the CLK source for LPTMR will be from external RTC_CLKIN as Mr Yasuhiko pointed out, pls refer to section 3.8.3.3 LPTMR prescaler/glitch filter clocking options in RM of KL04. But if you use RTC_CLKIN pin, you have to enable PORTA clock in SIM_SCGC5 and set the PORTB_PCR4 = 0x00000100; and set the SIM_SOPT1 =0x80000;&lt;/P&gt;&lt;P&gt;I have developed the code based on the FRDM-KL02 board, with which I can enter the LPTimer_IRQHandler(void) with 1KHz LPO clock source, you can copy the code directly for KL04.&lt;/P&gt;&lt;P&gt;I attach the code, hope it can help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Jan 2015 07:03:18 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2015-01-14T07:03:18Z</dc:date>
    <item>
      <title>ISR code not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336136#M16027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Friends,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an unusual problem :smileyhappy:&lt;/P&gt;&lt;P&gt;I have designed 3 boards (variants of he same app) using the KL04 chip. Now the code used is this -&lt;/P&gt;&lt;P&gt;#include "derivative.h" /* include peripheral declarations */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;//void UART0_IRQHandler(void);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// extern void LPTimer_IRQ(void);&lt;/P&gt;&lt;P&gt;// void LPTimer_IRQ(void);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int count;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint16_t countTemp = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; // asm(" CPSIE i");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCG_C1 |= 0x02;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SOPT1 = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC5 |= (SIM_SCGC5_LPTMR_MASK | SIM_SCGC5_PORTB_MASK);//PORTC_PCR1 |= PORT_PCR_MUX(1);//select RTC_CLKIN function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTB_PCR3 |= 0x00000100;&amp;nbsp;&amp;nbsp;&amp;nbsp; // alternative pin mux selection //&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PDDR |= 0x00000008;&amp;nbsp;&amp;nbsp;&amp;nbsp; // pin direction //&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTB_PCR4 |= 0x00000100;&amp;nbsp;&amp;nbsp;&amp;nbsp; // alternative pin mux selection //&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PDDR |= 0x00000010;&amp;nbsp;&amp;nbsp;&amp;nbsp; // pin direction //&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NVIC_ICPR = 1 &amp;lt;&amp;lt; (28);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NVIC_ISER = 1 &amp;lt;&amp;lt; (28);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC5|=SIM_SCGC5_LPTMR_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Reset LPTMR settings */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SOPT1 = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC5 |= (SIM_SCGC5_LPTMR_MASK | SIM_SCGC5_PORTB_MASK);//PORTC_PCR1 |= PORT_PCR_MUX(1);//select RTC_CLKIN function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CSR=0;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CSR |= 0x00000040;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CMR = 600;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PTOR |= (1 &amp;lt;&amp;lt; 3);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PTOR |= (1 &amp;lt;&amp;lt; 4);&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PTOR |= (1 &amp;lt;&amp;lt; 3);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PTOR |= (1 &amp;lt;&amp;lt; 4);&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Start the timer */&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait for counter to reach compare value */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(1){&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if((LPTMR0_CSR &amp;amp; 0x00000080) == 0x00000080){&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CSR &amp;amp;= ~LPTMR_CSR_TEN_MASK;&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CSR |= 0x00000080;&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PTOR |= (1 &amp;lt;&amp;lt; 3);&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PTOR |= (1 &amp;lt;&amp;lt; 4);&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void LPTimer_IRQHandler(void){&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if((LPTMR0_CSR &amp;amp; 0x00000080) == 0x00000080){&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CSR &amp;amp;= ~LPTMR_CSR_TEN_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CSR |= 0x00000080;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PTOR |= (1 &amp;lt;&amp;lt; 3);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PTOR |= (1 &amp;lt;&amp;lt; 4);&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ideally the controller should be interrupted and the control should go to the ISR (void LPTimer_IRQHandler(void)). What I see here is that in the 1st and the 2nd version of the board the ISR works well. But in the 3rd it doesnt. So, to test the 3rd board I made a pin toggle which is executed fine making me feel that this is a purely software issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a bit confused as to how this is being done.&lt;/P&gt;&lt;P&gt;I am stating the part number in all the 3 boards -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) -&amp;nbsp; M04R4V&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4EYIDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) M04R5V&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4EYIDM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) M04R5V&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ASAUK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me pls&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jan 2015 14:49:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336136#M16027</guid>
      <dc:creator>vinkar</dc:creator>
      <dc:date>2015-01-12T14:49:09Z</dc:date>
    </item>
    <item>
      <title>Re: ISR code not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336137#M16028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi vinod,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess your board has neither EXTAL0 nor XTAL0 oscillator. In the case, the setting SIM_SOPT1 0 would not select any clock for LPTMR. How about 0x000c0000 (i.e. LPO) as SIM_SOPT1 value? Also you should better make the first LPTMR0_CSR setting not 0 but 0x80 to clear the interrupt. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Yasuhiko Koumoto.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 06:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336137#M16028</guid>
      <dc:creator>yasuhikokoumoto</dc:creator>
      <dc:date>2015-01-13T06:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: ISR code not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336138#M16029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Vinod,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question, I have not the FRDM-KL04 board on hand, but I have FRDM-KL02Z board, I have tested the code on my FRDM-KL02Z board, I found out that the LPTMR0_PSR[PCS]=11 in binary for unknown reason&amp;nbsp; in default state, in the case, it selects the OSCERCLK as clock source, in the case, you should set the OSC32KSEL in SIM_SOPT1 as 10 in binary, in the setting, the CLK source for LPTMR will be from external RTC_CLKIN as Mr Yasuhiko pointed out, pls refer to section 3.8.3.3 LPTMR prescaler/glitch filter clocking options in RM of KL04. But if you use RTC_CLKIN pin, you have to enable PORTA clock in SIM_SCGC5 and set the PORTB_PCR4 = 0x00000100; and set the SIM_SOPT1 =0x80000;&lt;/P&gt;&lt;P&gt;I have developed the code based on the FRDM-KL02 board, with which I can enter the LPTimer_IRQHandler(void) with 1KHz LPO clock source, you can copy the code directly for KL04.&lt;/P&gt;&lt;P&gt;I attach the code, hope it can help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 07:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336138#M16029</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-01-14T07:03:18Z</dc:date>
    </item>
    <item>
      <title>Re: ISR code not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336139#M16030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Friends,&lt;/P&gt;&lt;P&gt;Thank you very much indeed for your responses.&lt;/P&gt;&lt;P&gt;I sincerely appreciate it.&lt;/P&gt;&lt;P&gt;SO with my code what I am doing is I am making the clock for the LPTMR come from RTC_CLKIN. And since I dont have such a clock its not working. So its all software.&lt;/P&gt;&lt;P&gt;But then how can it be explained that the LPTMR works for my older boards which also doesnt have the RTC_CLKIN. The code is completely the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vinod.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 13:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336139#M16030</guid>
      <dc:creator>vinkar</dc:creator>
      <dc:date>2015-01-14T13:04:40Z</dc:date>
    </item>
    <item>
      <title>Re: Re: ISR code not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336140#M16031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Vinod,&lt;/P&gt;&lt;P&gt;as you know, multiple clock source can drive the LPTMR, pls check the LPTMR0_PSR[PCS] to determine the clock source the LPTMR uses for your old code, I guess the LPTMR uses LPO, whatever.&lt;/P&gt;&lt;P&gt;Pls refer to the section I copied from UM of KL04.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48974i548931DCEBEA1A58/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jan 2015 03:09:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336140#M16031</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-01-15T03:09:55Z</dc:date>
    </item>
    <item>
      <title>Re: ISR code not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336141#M16032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xiangjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand ur point. But then how come it works in the other board but not i the new one.&lt;/P&gt;&lt;P&gt;Will nmi_b pin cause any mischief.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vinod&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 09:19:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ISR-code-not-working/m-p/336141#M16032</guid>
      <dc:creator>vinkar</dc:creator>
      <dc:date>2015-02-09T09:19:25Z</dc:date>
    </item>
  </channel>
</rss>