<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K60n512 SPI0 stress test issue in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60n512-SPI0-stress-test-issue/m-p/149388#M160</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Muffinman,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You have two K60's connected together using SPI0 on each one.&lt;/P&gt;&lt;P&gt;One K60 sends incrementing numbers from 0x00 to 0xff to the other, and then repeats&lt;/P&gt;&lt;P&gt;Eventually there are repeating failures at for expected data: x00 x7f x80 x81and xff.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However it does run fine for a while before these errors occur.&lt;/P&gt;&lt;P&gt;It also runs for a period of time between errors?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you post the data that is actually received vs the data that is expected?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Mar 2012 01:25:38 GMT</pubDate>
    <dc:creator>iafg</dc:creator>
    <dc:date>2012-03-28T01:25:38Z</dc:date>
    <item>
      <title>K60n512 SPI0 stress test issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60n512-SPI0-stress-test-issue/m-p/149387#M159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone meet the problem of SPI0 communication issue for stress test?&lt;/P&gt;&lt;P&gt;Let the two K60's SPI0 connect together, keep send increased data at 12M Hz.&lt;/P&gt;&lt;P&gt;After a while, there will be error received at 0xff, 0x7f, 0x00, 0x 80, 0x81?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2012 23:47:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60n512-SPI0-stress-test-issue/m-p/149387#M159</guid>
      <dc:creator>Muffinman</dc:creator>
      <dc:date>2012-03-27T23:47:53Z</dc:date>
    </item>
    <item>
      <title>Re: K60n512 SPI0 stress test issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60n512-SPI0-stress-test-issue/m-p/149388#M160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Muffinman,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You have two K60's connected together using SPI0 on each one.&lt;/P&gt;&lt;P&gt;One K60 sends incrementing numbers from 0x00 to 0xff to the other, and then repeats&lt;/P&gt;&lt;P&gt;Eventually there are repeating failures at for expected data: x00 x7f x80 x81and xff.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However it does run fine for a while before these errors occur.&lt;/P&gt;&lt;P&gt;It also runs for a period of time between errors?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you post the data that is actually received vs the data that is expected?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2012 01:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60n512-SPI0-stress-test-issue/m-p/149388#M160</guid>
      <dc:creator>iafg</dc:creator>
      <dc:date>2012-03-28T01:25:38Z</dc:date>
    </item>
    <item>
      <title>Re: K60n512 SPI0 stress test issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60n512-SPI0-stress-test-issue/m-p/149389#M161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe related to this post too??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/99898#99898" title="https://community.freescale.com/message/99898#99898"&gt;https://community.freescale.com/message/99898#99898&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2012 01:40:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60n512-SPI0-stress-test-issue/m-p/149389#M161</guid>
      <dc:creator>iafg</dc:creator>
      <dc:date>2012-03-28T01:40:20Z</dc:date>
    </item>
    <item>
      <title>Re: K60n512 SPI0 stress test issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60n512-SPI0-stress-test-issue/m-p/149390#M162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I paste the error reading there:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;.Master Read Error: ff : 0&lt;BR /&gt;.Master Read: ff : 745 ms&lt;BR /&gt;.&lt;BR /&gt;.Master Read: 0 : 7636 ms&lt;BR /&gt;.&lt;BR /&gt;.Master Read: 1 : 7637 ms&lt;BR /&gt;.&lt;BR /&gt;.Master Read Error: ff : c4&lt;BR /&gt;.Master Read Error: c7 : 0&lt;BR /&gt;.Master Read: 2 : 839 ms&lt;BR /&gt;.&lt;BR /&gt;.Master Read: 3 : 7639 ms&lt;BR /&gt;.&lt;BR /&gt;.Master Read: 4 : 7639 ms&lt;BR /&gt;.&lt;BR /&gt;.Master Read: 5 : 639 ms&lt;BR /&gt;.&lt;BR /&gt;.Master Read: 6 : 7639 ms&lt;BR /&gt;.&lt;BR /&gt;.Master Read: 7 : 7640 ms&lt;BR /&gt;.&lt;BR /&gt;.Master Read: 8 : 639 ms&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTW:&lt;/P&gt;&lt;P&gt;Between each two master reading, there will be couple hudreds K bytes transmit/receive, the master read error happen between the two master reading formated with Master Read Error: Real read value: Should read value.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2012 20:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60n512-SPI0-stress-test-issue/m-p/149390#M162</guid>
      <dc:creator>Muffinman</dc:creator>
      <dc:date>2012-03-28T20:28:17Z</dc:date>
    </item>
  </channel>
</rss>