<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Disabling External PullUp in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disabling-External-PullUp/m-p/177731#M1580</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm learning about MQX... but I have a simple problem... how can I change the registry to disable internal pull-up for a GPIO?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using PORTC_PCR10 as digital input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Oct 2011 05:48:52 GMT</pubDate>
    <dc:creator>infinity</dc:creator>
    <dc:date>2011-10-28T05:48:52Z</dc:date>
    <item>
      <title>Disabling External PullUp</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disabling-External-PullUp/m-p/177731#M1580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm learning about MQX... but I have a simple problem... how can I change the registry to disable internal pull-up for a GPIO?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using PORTC_PCR10 as digital input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2011 05:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disabling-External-PullUp/m-p/177731#M1580</guid>
      <dc:creator>infinity</dc:creator>
      <dc:date>2011-10-28T05:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: Disabling External PullUp</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disabling-External-PullUp/m-p/177732#M1581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this not a question for the Kinetis?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Coldfires have fixed internal pullups (where present) which are enabled by default.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Kinetis allows configuration of pull-up/down or none.&lt;/P&gt;&lt;P&gt;If you write 0x00000100 to the corresponding PCR register the pin will be configured as GPIO - as input it has no pullup/down.&lt;/P&gt;&lt;P&gt;The pullup/down is only enabled when 0x00000002 is set as well whereby the bit 0x00000001 controls whether this is pullup or pull down.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2011 07:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disabling-External-PullUp/m-p/177732#M1581</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-10-28T07:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: Disabling External PullUp</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disabling-External-PullUp/m-p/177733#M1582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Oh yes&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;it is true&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;I put&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;the post&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;in the wrong section&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using TWRK40_512.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;do I move&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;my post? Please some admin can do this for me?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;I still have&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;problems&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;I set&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;as you said&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;PORTC_PCR10&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But&lt;/SPAN&gt;&amp;nbsp;it seems that&amp;nbsp;&lt;SPAN&gt;there&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;is&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;some function&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;call that&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;overwrite&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;this&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;setting&lt;/SPAN&gt;&amp;nbsp;and then r&lt;SPAN&gt;eactivate&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;the&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;pull&lt;/SPAN&gt;&lt;SPAN&gt;-&lt;/SPAN&gt;&lt;SPAN&gt;up&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;...&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;why&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;this&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;behavior?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2011 18:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disabling-External-PullUp/m-p/177733#M1582</guid>
      <dc:creator>infinity</dc:creator>
      <dc:date>2011-10-28T18:11:19Z</dc:date>
    </item>
    <item>
      <title>Re: Disabling External PullUp</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disabling-External-PullUp/m-p/177734#M1583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This sounds like a software issue so it depends on the SW that you are using.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Try puttiung a breakpoint on write accesses to the register to see where it is being written from&lt;/P&gt;&lt;P&gt;2) Or, write the value that you want later (after the unknown function has done its work).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2011 22:53:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Disabling-External-PullUp/m-p/177734#M1583</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-10-28T22:53:01Z</dc:date>
    </item>
  </channel>
</rss>