<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK10 - OK to use flash below 0x400?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-OK-to-use-flash-below-0x400/m-p/333577#M15786</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running really low on flash space on a MK10DN32VFM5 and am looking for somewhere for a field write-once array.&lt;/P&gt;&lt;P&gt;The device only has 62 interrupt vectors so the space from 0x0F8-0x3FF looks to be unused.&lt;/P&gt;&lt;P&gt;I've tried creating a linker section here, putting an array in it and it seems to work fine.&lt;/P&gt;&lt;P&gt;Is it OK to use this section? I can't find anything in the datasheet that says whether it is or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Feb 2015 15:23:14 GMT</pubDate>
    <dc:creator>chris_f</dc:creator>
    <dc:date>2015-02-24T15:23:14Z</dc:date>
    <item>
      <title>K10 - OK to use flash below 0x400?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-OK-to-use-flash-below-0x400/m-p/333577#M15786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running really low on flash space on a MK10DN32VFM5 and am looking for somewhere for a field write-once array.&lt;/P&gt;&lt;P&gt;The device only has 62 interrupt vectors so the space from 0x0F8-0x3FF looks to be unused.&lt;/P&gt;&lt;P&gt;I've tried creating a linker section here, putting an array in it and it seems to work fine.&lt;/P&gt;&lt;P&gt;Is it OK to use this section? I can't find anything in the datasheet that says whether it is or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2015 15:23:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-OK-to-use-flash-below-0x400/m-p/333577#M15786</guid>
      <dc:creator>chris_f</dc:creator>
      <dc:date>2015-02-24T15:23:14Z</dc:date>
    </item>
    <item>
      <title>Re: K10 - OK to use flash below 0x400?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-OK-to-use-flash-below-0x400/m-p/333578#M15787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As long as you respect the normal Flash writing rules there is no problem using free space in the first sector for saving write-once parameters to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;K20: &lt;A href="http://www.utasker.com/kinetis/TWR-K20D72M.html" title="http://www.utasker.com/kinetis/TWR-K20D72M.html"&gt;µTasker Kinetis TWR-K20D72M support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/FRDM-K20D50M.html" title="http://www.utasker.com/kinetis/FRDM-K20D50M.html"&gt;µTasker Kinetis FRDM-K20D50M support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/FRDM-K20D50M.html" title="http://www.utasker.com/kinetis/FRDM-K20D50M.html"&gt;µTasker Kinetis FRDM-K20D50M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2015 15:32:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-OK-to-use-flash-below-0x400/m-p/333578#M15787</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-02-24T15:32:05Z</dc:date>
    </item>
    <item>
      <title>Re: K10 - OK to use flash below 0x400?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-OK-to-use-flash-below-0x400/m-p/333579#M15788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Excellent. Thanks for the fast reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2015 15:33:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-OK-to-use-flash-below-0x400/m-p/333579#M15788</guid>
      <dc:creator>chris_f</dc:creator>
      <dc:date>2015-02-24T15:33:57Z</dc:date>
    </item>
  </channel>
</rss>