<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Running a K6x from external Flash via the Flexbus. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Running-a-K6x-from-external-Flash-via-the-Flexbus/m-p/332790#M15708</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Allan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using FlexBus it is able to perform 16-bit and 32-bit reads and writes using 16-bit and 32-bit interface. So, it does not matter if you use 16-bit or 32-bit interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Technical Support Engineer&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Feb 2015 23:48:56 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2015-02-24T23:48:56Z</dc:date>
    <item>
      <title>Running a K6x from external Flash via the Flexbus.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Running-a-K6x-from-external-Flash-via-the-Flexbus/m-p/332789#M15707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When running a K6x from external NOR flash, should the flash interface be 16 bit or 32 bit, or can it be either? Is the K6X (thumb only) even capable of running code from 32bit external Flash memory?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2015 11:28:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Running-a-K6x-from-external-Flash-via-the-Flexbus/m-p/332789#M15707</guid>
      <dc:creator>allandimmock</dc:creator>
      <dc:date>2015-02-24T11:28:37Z</dc:date>
    </item>
    <item>
      <title>Re: Running a K6x from external Flash via the Flexbus.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Running-a-K6x-from-external-Flash-via-the-Flexbus/m-p/332790#M15708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Allan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using FlexBus it is able to perform 16-bit and 32-bit reads and writes using 16-bit and 32-bit interface. So, it does not matter if you use 16-bit or 32-bit interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Technical Support Engineer&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2015 23:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Running-a-K6x-from-external-Flash-via-the-Flexbus/m-p/332790#M15708</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2015-02-24T23:48:56Z</dc:date>
    </item>
  </channel>
</rss>