<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK10D input protection diode</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332308#M15607</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The PTC1 pin on the K10D is configured for input capture function, but it also has an alternate analog function which is not used in the design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the input protection to VDD through a clamping diode still available when configured for input capture, or just when the pin is configured as an analog function?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What kind of internal protection is offered on the default Port IO pins?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Nov 2014 21:57:39 GMT</pubDate>
    <dc:creator>ScottKerstein</dc:creator>
    <dc:date>2014-11-11T21:57:39Z</dc:date>
    <item>
      <title>K10D input protection diode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332308#M15607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The PTC1 pin on the K10D is configured for input capture function, but it also has an alternate analog function which is not used in the design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the input protection to VDD through a clamping diode still available when configured for input capture, or just when the pin is configured as an analog function?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What kind of internal protection is offered on the default Port IO pins?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Nov 2014 21:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332308#M15607</guid>
      <dc:creator>ScottKerstein</dc:creator>
      <dc:date>2014-11-11T21:57:39Z</dc:date>
    </item>
    <item>
      <title>Re: K10D input protection diode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332309#M15608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any pin that CAN be GPIO physically does NOT have said diode to VDD, and can accept -0.3 to 5.5V at any time, in any mode.&amp;nbsp; The protection elements do not change based on 'pin mode'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Nov 2014 15:39:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332309#M15608</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2014-11-12T15:39:24Z</dc:date>
    </item>
    <item>
      <title>Re: K10D input protection diode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332310#M15609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ESD protection circuit (clamping diode) is applied for each port IO pin, whatever it configured for input capture or analog function.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Nov 2014 07:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332310#M15609</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-11-13T07:52:34Z</dc:date>
    </item>
    <item>
      <title>Re: K10D input protection diode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332311#M15610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks.&amp;nbsp; It appears the other I/O isn't protect.&amp;nbsp; Why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Nov 2014 22:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332311#M15610</guid>
      <dc:creator>ScottKerstein</dc:creator>
      <dc:date>2014-11-13T22:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: K10D input protection diode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332312#M15611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not sure "the other I/O" means?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Nov 2014 02:50:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332312#M15611</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-11-14T02:50:32Z</dc:date>
    </item>
    <item>
      <title>Re: K10D input protection diode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332313#M15612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no diode to VDD on all GPIO-capable pins to allow 5V input signal level tolerance, irrespective of actual Vdd voltage.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Nov 2014 03:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332313#M15612</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2014-11-14T03:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: K10D input protection diode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332314#M15613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the 5V tolerant I/O with special design, the diode not connect to VDD, while instead to a ESD Bus.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Nov 2014 08:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10D-input-protection-diode/m-p/332314#M15613</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-11-17T08:29:33Z</dc:date>
    </item>
  </channel>
</rss>