<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis K64 Ethernet in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ethernet/m-p/328923#M15245</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Use the FRDM-K64F circuit diagram as reference.&lt;/P&gt;&lt;P&gt;It connects the EXTAL0 to the PHY's 50MHz REF_CLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make sure that you use the KS8081&lt;STRONG&gt;RNA&lt;/STRONG&gt; (generates 50MHz clock form 25MHz crystal) and not the KS8081&lt;STRONG&gt;RND&lt;/STRONG&gt; (which requires a 50MHz clock)!!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Sep 2014 15:05:08 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-09-18T15:05:08Z</dc:date>
    <item>
      <title>Kinetis K64 Ethernet</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ethernet/m-p/328922#M15244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using K64 microcontroller and I need to implement Ethernet , hence I'm using suggested PHY KSZ8081 and RJ45 JX0011D21NL .I want to know how to conenct REF_CLK with microprocessor as pin 72 ( PTA18/EXTAL0/FTM0_FLT2/FTM_CLKIN0 ) is being used by external oscillator to provide clock to microprocessor.&lt;/P&gt;&lt;P&gt;Can someone tell me how to set clock for syncing ethernet PHY and microprocessor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 14:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ethernet/m-p/328922#M15244</guid>
      <dc:creator>punyatagayatri</dc:creator>
      <dc:date>2014-09-18T14:28:04Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 Ethernet</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ethernet/m-p/328923#M15245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Use the FRDM-K64F circuit diagram as reference.&lt;/P&gt;&lt;P&gt;It connects the EXTAL0 to the PHY's 50MHz REF_CLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make sure that you use the KS8081&lt;STRONG&gt;RNA&lt;/STRONG&gt; (generates 50MHz clock form 25MHz crystal) and not the KS8081&lt;STRONG&gt;RND&lt;/STRONG&gt; (which requires a 50MHz clock)!!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 15:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ethernet/m-p/328923#M15245</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-09-18T15:05:08Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 Ethernet</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ethernet/m-p/328924#M15246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using a cystal to program the microprocessor at this pin so its occupied.Is there any provision to synchronise MAC of processor with PHY Ref Clock.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Sep 2014 06:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ethernet/m-p/328924#M15246</guid>
      <dc:creator>punyatagayatri</dc:creator>
      <dc:date>2014-09-19T06:57:23Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 Ethernet</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ethernet/m-p/328925#M15247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an alternative clock source for ENET module, you may feed ENET_1588_CLKIN with 50MHz clock as the same as PHY Ref Clock. Please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47120i35748E86F5BDDE20/image-size/large?v=v2&amp;amp;px=999" title="Untitled.png" alt="Untitled.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 07:04:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ethernet/m-p/328925#M15247</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-11-10T07:04:37Z</dc:date>
    </item>
  </channel>
</rss>