<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: compiling CAU and mmCAU library with Freescale compiler - errors in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/compiling-CAU-and-mmCAU-library-with-Freescale-compiler-errors/m-p/328662#M15217</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello martinpi:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you still have this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not used the mmcau library, but I think the assembly code should be compatible with both compilers.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Dec 2014 21:10:41 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2014-12-16T21:10:41Z</dc:date>
    <item>
      <title>compiling CAU and mmCAU library with Freescale compiler - errors</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/compiling-CAU-and-mmCAU-library-with-Freescale-compiler-errors/m-p/328661#M15216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have an existing Kinetis Project and need to add an MD5 calculation.&lt;/P&gt;&lt;P&gt;I added the CAU/mmCAU library and got lots of errors when I tried to compile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Created a new bareboard project, this time using GCC instead of Freescale compiler, &lt;BR /&gt;and it compiled (i.e. assembled) smoothly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The existing project is compiled with Freescale compiler and not with GCC.&lt;/P&gt;&lt;P&gt;It will not compile with GCC, and we have to use the Freescale compiler for legal reasons.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I compile the CAU/mmCAU library under Freescale compiler?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2014 14:00:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/compiling-CAU-and-mmCAU-library-with-Freescale-compiler-errors/m-p/328661#M15216</guid>
      <dc:creator>martinpi</dc:creator>
      <dc:date>2014-12-05T14:00:30Z</dc:date>
    </item>
    <item>
      <title>Re: compiling CAU and mmCAU library with Freescale compiler - errors</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/compiling-CAU-and-mmCAU-library-with-Freescale-compiler-errors/m-p/328662#M15217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello martinpi:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you still have this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not used the mmcau library, but I think the assembly code should be compatible with both compilers.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2014 21:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/compiling-CAU-and-mmCAU-library-with-Freescale-compiler-errors/m-p/328662#M15217</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-12-16T21:10:41Z</dc:date>
    </item>
    <item>
      <title>Re: compiling CAU and mmCAU library with Freescale compiler - errors</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/compiling-CAU-and-mmCAU-library-with-Freescale-compiler-errors/m-p/328663#M15218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for answering.&lt;/P&gt;&lt;P&gt;The readme says that the sources have been compiled with GCC,&lt;/P&gt;&lt;P&gt;and it simply does not compile with CW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But there is a compiled library enclosed in the download (I thought it is an additional library to be linked with the assembly code, but it is the same binary which I get when I compile the assembly code with GCC).&lt;/P&gt;&lt;P&gt;So, I do not need to compile but use the binary provided. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2015 08:57:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/compiling-CAU-and-mmCAU-library-with-Freescale-compiler-errors/m-p/328663#M15218</guid>
      <dc:creator>martinpi</dc:creator>
      <dc:date>2015-01-05T08:57:15Z</dc:date>
    </item>
  </channel>
</rss>