<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FRDM-K64F RTC working?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-RTC-working/m-p/327600#M15135</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, once the setup was right, I can detect the 32K oscillation. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Oct 2014 20:57:53 GMT</pubDate>
    <dc:creator>haizhouli</dc:creator>
    <dc:date>2014-10-15T20:57:53Z</dc:date>
    <item>
      <title>FRDM-K64F RTC working?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-RTC-working/m-p/327598#M15133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using FRDM-K64F as a prototype board for RTC test.&amp;nbsp; I used PE to program rtc, but the clock seems not running. I am using an oscilloscope to check the 32K crystal. I can see both the 8MHz and 25Mhz on board. But no oscillation on 32K crystal at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone worked on FRDM-K64F RTC before? I had three FRDM boards and none has oscillation. Do I need pop those caps and resistors based on the schematics&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Haizhou &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Oct 2014 16:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-RTC-working/m-p/327598#M15133</guid>
      <dc:creator>haizhouli</dc:creator>
      <dc:date>2014-10-15T16:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F RTC working?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-RTC-working/m-p/327599#M15134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is not necessary to add any capacitors to use the RTC:&lt;/P&gt;&lt;P&gt;Make sure that the RTC uis powered up (RTC bit in SIM_SCGC6) and its clock source correctly selected (in RTC_SC) and enabled in RTC_CR. The DC level on the pins will then increase form 0V to about mid-voltage and the 32kHz will be present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Oct 2014 16:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-RTC-working/m-p/327599#M15134</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-10-15T16:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F RTC working?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-RTC-working/m-p/327600#M15135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, once the setup was right, I can detect the 32K oscillation. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Oct 2014 20:57:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-RTC-working/m-p/327600#M15135</guid>
      <dc:creator>haizhouli</dc:creator>
      <dc:date>2014-10-15T20:57:53Z</dc:date>
    </item>
  </channel>
</rss>