<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 5V tolerant digital inputs on K40? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176226#M1501</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone know if the ADC inputs on the Kinetis 40&amp;nbsp; series are 5V tolerant? The data says the digital I/Os only, not the analog inputs are 5V tolerant. The definition of analog is unclear - some of the ADC inputs have digital input options too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Aug 2012 16:02:34 GMT</pubDate>
    <dc:creator>stav</dc:creator>
    <dc:date>2012-08-08T16:02:34Z</dc:date>
    <item>
      <title>5V tolerant digital inputs on K60?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176222#M1497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are digital K60 I/O 5V tolerant when used as inputs?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the datasheet the Absolute Maximum Rating is -0.3V to +5.5V, so it seems it would be safe to interface a 5V signal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What do you think?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2012 21:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176222#M1497</guid>
      <dc:creator>pozz</dc:creator>
      <dc:date>2012-06-29T21:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: 5V tolerant digital inputs on K60?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176223#M1498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think that's fine, but I haven't actually tried it myself.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jul 2012 16:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176223#M1498</guid>
      <dc:creator>OliverSedlacek</dc:creator>
      <dc:date>2012-07-02T16:19:38Z</dc:date>
    </item>
    <item>
      <title>Re: 5V tolerant digital inputs on K60?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176224#M1499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anyone from Freescale can confirm?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jul 2012 16:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176224#M1499</guid>
      <dc:creator>pozz</dc:creator>
      <dc:date>2012-07-02T16:29:57Z</dc:date>
    </item>
    <item>
      <title>Re: 5V tolerant digital inputs on K60?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176225#M1500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;"All 5 volt tolerant digital I/O pins are internally clamped to VSS through a ESD protection diode. There is no diode connection to VDD." So yes, they are 5V tolerant. You just have to find out which of the I/O pins are 5V tolerant.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jul 2012 17:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176225#M1500</guid>
      <dc:creator>Burba</dc:creator>
      <dc:date>2012-07-05T17:54:48Z</dc:date>
    </item>
    <item>
      <title>Re: 5V tolerant digital inputs on K40?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176226#M1501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone know if the ADC inputs on the Kinetis 40&amp;nbsp; series are 5V tolerant? The data says the digital I/Os only, not the analog inputs are 5V tolerant. The definition of analog is unclear - some of the ADC inputs have digital input options too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Aug 2012 16:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/5V-tolerant-digital-inputs-on-K60/m-p/176226#M1501</guid>
      <dc:creator>stav</dc:creator>
      <dc:date>2012-08-08T16:02:34Z</dc:date>
    </item>
  </channel>
</rss>