<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Is it possible to read a single ended input on a DMx input pin?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-read-a-single-ended-input-on-a-DMx-input-pin/m-p/325129#M14893</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All devices allow ADC0_DM0 as single ended ADC input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To be absolutely sure I just connected the ADC0_DM0 input to the potentiometer wiper on the TWR-K40x256 board and compared the values read from ADC0_DM0 and ADC1_DM1 (both set up for single-ended operation) and the two ADC samples for the two inputs followed each other (to within 2 noise bits) across the potentiometer range (0x0000..0x0ffff).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jun 2014 23:23:42 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-06-26T23:23:42Z</dc:date>
    <item>
      <title>Is it possible to read a single ended input on a DMx input pin?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-read-a-single-ended-input-on-a-DMx-input-pin/m-p/325128#M14892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; I'm using the K40X256 tower board and one of the backemf signals from the 3phase motor board goes to ADC0_DM0 and I need to read it.&amp;nbsp; Processor expert warns me if I try to configure channel 0 as a single ended input but nothing in the datasheet I see indicates that channel 0 is differential-only.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 21:44:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-read-a-single-ended-input-on-a-DMx-input-pin/m-p/325128#M14892</guid>
      <dc:creator>robotjosh</dc:creator>
      <dc:date>2014-06-26T21:44:22Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to read a single ended input on a DMx input pin?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-read-a-single-ended-input-on-a-DMx-input-pin/m-p/325129#M14893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All devices allow ADC0_DM0 as single ended ADC input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To be absolutely sure I just connected the ADC0_DM0 input to the potentiometer wiper on the TWR-K40x256 board and compared the values read from ADC0_DM0 and ADC1_DM1 (both set up for single-ended operation) and the two ADC samples for the two inputs followed each other (to within 2 noise bits) across the potentiometer range (0x0000..0x0ffff).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 23:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-read-a-single-ended-input-on-a-DMx-input-pin/m-p/325129#M14893</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-26T23:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to read a single ended input on a DMx input pin?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-read-a-single-ended-input-on-a-DMx-input-pin/m-p/325130#M14894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you set it up with processor expert adc_init?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Josh Jordan&lt;/P&gt;&lt;P&gt;Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2014 16:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-read-a-single-ended-input-on-a-DMx-input-pin/m-p/325130#M14894</guid>
      <dc:creator>robotjosh</dc:creator>
      <dc:date>2014-06-27T16:22:27Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to read a single ended input on a DMx input pin?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-read-a-single-ended-input-on-a-DMx-input-pin/m-p/325131#M14895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No - I just used the uTasker project since it supports the ADCs in interrupt and DMA mode on all K and KL boards (just selected the K40 TWR target and changed one line of code to select the input you asked about).&lt;/P&gt;&lt;P&gt;Try ignoring the warning (PE may have bugs and limitiations) and see whether it works or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2014 16:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-read-a-single-ended-input-on-a-DMx-input-pin/m-p/325131#M14895</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-27T16:42:16Z</dc:date>
    </item>
  </channel>
</rss>