<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Re: Can't boot TWR-K60N512 standalone... in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324813#M14842</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I loaded your code to my TWR board and I am 99% sure it is due to the watchdog not being configured early enough.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your code starts at 0x0439 (the first instruction executed) and the very first thing that it does is initialise variables. In this case it has 0x970 variables to be initialised (this is a loop copying const values from Flash at 0xd6e8 to the RAM area 0x1fff0410..0x1fff0d80 [initialised variables]). In fact it copies always long words starting at the end of the area and working backwards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a breakpoint is set "after" this loop [address 0x44a]&amp;nbsp; it will never be reached - there is a reset before it gets that far.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a memory fill is performed in the RAM area before starting it is seen that the loop manages to copy 32 long words before the reset takes place since the FLASH values are seen to have been written there).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When working with the debugger the results can be a bit different - by setting a breakpoint in the loop itself it was in fact possible to run to the break point in each loop cycle and it managed many loops without the reset taking place.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn't see any code that configures the watchog (there is a routine called monWatchDog but looks to not be doing any initialisation). Therefore I couldn't try jumping to code that disables the watchdog and then jumping back to the initialisation to see whether the code then actually ran successfully. Since the requirements for unlocking and disabling the watchdog are very critical it is not posssible to do it manually.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using code that initialises variables before configuring the watchdog may work if there are only a few variables to be initialsied but when the operation exceeds the 256 allowed instructions it would then fail (eg. when a few more variables are added).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't explain why the debugger allows the code to operate but, as stated above, I believe the only way to do this is to put the watchog initisation "before" any variable initialisation since it is "normal" (from experience and written references) that if the 256 instructions are used up the watchdog will fire and so the code can't operate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jun 2014 18:02:57 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-06-26T18:02:57Z</dc:date>
    <item>
      <title>Can't boot TWR-K60N512 standalone...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324806#M14835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been building a small app on a TWR-K60N512 (includes the serial card) for several days using a Segger JLink programmer connected to the 20-pin debug header.&amp;nbsp; This has been working just fine.&amp;nbsp; Now I tried removing the programmer to allow the board to run standalone and it doesn't boot.&amp;nbsp; I'm not using the JLINK for power (J13/USB does that); so I'm confused.&lt;/P&gt;&lt;P&gt;With JLINK attached, I can power cycle the board and then just run a JLINK script (see below) to restart it and that works fine; so that tells me that the boot flash is properly programmed (doesn't it?).&lt;/P&gt;&lt;P&gt;I noticed that with the JLINK attached, the "RESET" button on the TWR-K60N512 also just locks up the board (I assume it goes to the same "space" as a powerup).&amp;nbsp; Any ideas what I might be doing wrong?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;JLINK reset script:&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: 'courier new', courier;"&gt;device=MK60DN512xxx10&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: 'courier new', courier;"&gt;speed auto&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: 'courier new', courier;"&gt;r&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: 'courier new', courier;"&gt;h&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: 'courier new', courier;"&gt;go&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: 'courier new', courier;"&gt;exit&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 12:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324806#M14835</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2014-06-26T12:06:48Z</dc:date>
    </item>
    <item>
      <title>Re: Can't boot TWR-K60N512 standalone...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324807#M14836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it a watchdog issue? Ensure that the watchdog is either disabled or configured within 256 clock cycles (maybe the debugger is handling this too):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf" title="http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf"&gt;http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf&lt;/A&gt; (page 33)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/forum/index.php?topic=1664.0" title="http://www.utasker.com/forum/index.php?topic=1664.0"&gt;http://www.utasker.com/forum/index.php?topic=1664.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 15:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324807#M14836</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-26T15:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: Can't boot TWR-K60N512 standalone...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324808#M14837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ed:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You do not mention the IDE/toolchain, but just in case you use CodeWarrior we have seen this problem before, check the next thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/391776"&gt;Re: MK10DX256VLK7 doesn't run standalone, just when debugging. Verified it's running from FLASH, not RAM.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 15:34:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324808#M14837</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-06-26T15:34:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can't boot TWR-K60N512 standalone...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324809#M14838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mark,&lt;/P&gt;&lt;P&gt;I don't *think* thats a problem.&amp;nbsp; I've booted a K64F FRDM board prior to this with similar startup.&lt;/P&gt;&lt;P&gt;I disable the watchdog in SystemInit()..&amp;nbsp; Strangely, there is something else to add, based on your&lt;/P&gt;&lt;P&gt;watchdog suggestion...&lt;/P&gt;&lt;P&gt;I have a small reset function which enables the watchdog and just waits for it to kick in.&lt;/P&gt;&lt;P&gt;Based on your comment, I added a timeout to the wait loop that I have in there just to see&lt;/P&gt;&lt;P&gt;if its getting locked up in the while(1) (endlessly waiting for a reset to occur).&amp;nbsp; Its not timing out.&lt;/P&gt;&lt;P&gt;That tells me that the board actually is *trying* to reset, but is not successfully.&lt;/P&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 15:46:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324809#M14838</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2014-06-26T15:46:45Z</dc:date>
    </item>
    <item>
      <title>Re: Can't boot TWR-K60N512 standalone...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324810#M14839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jorge,&lt;/P&gt;&lt;P&gt;Not using any IDE; just gcc and Segger JLINK to burn the boot flash.&lt;/P&gt;&lt;P&gt;No semihosting involved here, my printf is directed to the serial port that is on&lt;/P&gt;&lt;P&gt;the TWR-SER card.&amp;nbsp; &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;I just use the USB port for power.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Ed&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 15:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324810#M14839</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2014-06-26T15:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: Can't boot TWR-K60N512 standalone...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324811#M14840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please post/attach your binary and MAP file.&lt;/P&gt;&lt;P&gt;I would be interested in checking what the Kinetis is doing in this case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 16:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324811#M14840</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-26T16:09:24Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Can't boot TWR-K60N512 standalone...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324812#M14841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mark,&lt;/P&gt;&lt;P&gt;Ok, here they are...&lt;/P&gt;&lt;P&gt;I included the .elf file as well.&lt;/P&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 17:02:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324812#M14841</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2014-06-26T17:02:16Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Can't boot TWR-K60N512 standalone...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324813#M14842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I loaded your code to my TWR board and I am 99% sure it is due to the watchdog not being configured early enough.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your code starts at 0x0439 (the first instruction executed) and the very first thing that it does is initialise variables. In this case it has 0x970 variables to be initialised (this is a loop copying const values from Flash at 0xd6e8 to the RAM area 0x1fff0410..0x1fff0d80 [initialised variables]). In fact it copies always long words starting at the end of the area and working backwards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a breakpoint is set "after" this loop [address 0x44a]&amp;nbsp; it will never be reached - there is a reset before it gets that far.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a memory fill is performed in the RAM area before starting it is seen that the loop manages to copy 32 long words before the reset takes place since the FLASH values are seen to have been written there).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When working with the debugger the results can be a bit different - by setting a breakpoint in the loop itself it was in fact possible to run to the break point in each loop cycle and it managed many loops without the reset taking place.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn't see any code that configures the watchog (there is a routine called monWatchDog but looks to not be doing any initialisation). Therefore I couldn't try jumping to code that disables the watchdog and then jumping back to the initialisation to see whether the code then actually ran successfully. Since the requirements for unlocking and disabling the watchdog are very critical it is not posssible to do it manually.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using code that initialises variables before configuring the watchdog may work if there are only a few variables to be initialsied but when the operation exceeds the 256 allowed instructions it would then fail (eg. when a few more variables are added).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't explain why the debugger allows the code to operate but, as stated above, I believe the only way to do this is to put the watchog initisation "before" any variable initialisation since it is "normal" (from experience and written references) that if the 256 instructions are used up the watchdog will fire and so the code can't operate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 18:02:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324813#M14842</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-26T18:02:57Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Can't boot TWR-K60N512 standalone...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324814#M14843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mark,&lt;/P&gt;&lt;P&gt;You're right!!! &lt;/P&gt;&lt;P&gt;After reading your response and looking at my code (again), I realized I moved my call&lt;/P&gt;&lt;P&gt;to SystemInit() (where I was disabling the WD) to a point much deeper in my startup.&lt;/P&gt;&lt;P&gt;I now do the watchdog disable &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;right out of the reset handler and it boots fine!!!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks very much!!&lt;/P&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS...&lt;/P&gt;&lt;P&gt;An interesting take-away from this is that somehow the SEGGER (or something that is associated &lt;/P&gt;&lt;P&gt;with that connection) magically disables the WD when connected.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 18:12:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-boot-TWR-K60N512-standalone/m-p/324814#M14843</guid>
      <dc:creator>EdSutter</dc:creator>
      <dc:date>2014-06-26T18:12:09Z</dc:date>
    </item>
  </channel>
</rss>