<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Header file for KL16</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Header-file-for-KL16/m-p/324694#M14833</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is the peripheral memory map header file the same for the KL26 and the KL16?&amp;nbsp; I can't find one for the KL16, which is what we're using, but the FRDM board says it's for both processors.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jul 2014 19:11:44 GMT</pubDate>
    <dc:creator>chuckh</dc:creator>
    <dc:date>2014-07-24T19:11:44Z</dc:date>
    <item>
      <title>Header file for KL16</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Header-file-for-KL16/m-p/324694#M14833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is the peripheral memory map header file the same for the KL26 and the KL16?&amp;nbsp; I can't find one for the KL16, which is what we're using, but the FRDM board says it's for both processors.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2014 19:11:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Header-file-for-KL16/m-p/324694#M14833</guid>
      <dc:creator>chuckh</dc:creator>
      <dc:date>2014-07-24T19:11:44Z</dc:date>
    </item>
    <item>
      <title>Re: Header file for KL16</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Header-file-for-KL16/m-p/324695#M14834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The difference between this two devices is that the KL26 has the support for the USB module and the KL16 has not. In the attachments you can find the header file for both processors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have installed CW 10.x you can find the header files for each processor in this path: &amp;lt;install_folder&amp;gt;\Freescale\CW MCU v10.6\MCU\lib\wizard_data\ARM\DataBase\derivatives&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. It would be nice!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2014 19:28:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Header-file-for-KL16/m-p/324695#M14834</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-07-24T19:28:36Z</dc:date>
    </item>
  </channel>
</rss>