<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using TSS_Library with MQX-Lite in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324201#M14822</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;What else should I do to fix this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vinícius Hoff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Aug 2014 12:37:14 GMT</pubDate>
    <dc:creator>ViniciusHoff</dc:creator>
    <dc:date>2014-08-12T12:37:14Z</dc:date>
    <item>
      <title>Using TSS_Library with MQX-Lite</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324197#M14818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a MQX-Lite project with four touch button, using the TSS_Library. When&lt;/P&gt;&lt;P&gt;I use the TSS_Library in MQX project, no button is detected and TSS1_fCallBack0 is never called. If I use the TSS_Library, with same configuration, in bareboard project, the buttons work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How I configure TSS_Library in MQX-Lite project?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jul 2014 17:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324197#M14818</guid>
      <dc:creator>ViniciusHoff</dc:creator>
      <dc:date>2014-07-23T17:59:31Z</dc:date>
    </item>
    <item>
      <title>Re: Using TSS_Library with MQX-Lite</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324198#M14819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using only a task in the MQX-project, with one loop where I call TSS_Task().&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2014 14:39:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324198#M14819</guid>
      <dc:creator>ViniciusHoff</dc:creator>
      <dc:date>2014-07-24T14:39:55Z</dc:date>
    </item>
    <item>
      <title>Re: Using TSS_Library with MQX-Lite</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324199#M14820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below threads and let me know if these help!!!&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/300301"&gt;Unable to find TSS_Library Component&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/300653"&gt;Configuring and Using K20 TSI with TSS_Library Component in a MQX application&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jul 2014 13:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324199#M14820</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-07-28T13:53:51Z</dc:date>
    </item>
    <item>
      <title>Re: Using TSS_Library with MQX-Lite</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324200#M14821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi soledad,&lt;/P&gt;&lt;P&gt;I read the threads and I followed the tips, but the touch buttons don't work yet.&lt;/P&gt;&lt;P&gt;If I use the same program without the MQX-Lite, TSS Library works well. Could be because of the call time of the MQX task?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Vinicius&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Aug 2014 13:44:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324200#M14821</guid>
      <dc:creator>ViniciusHoff</dc:creator>
      <dc:date>2014-08-05T13:44:06Z</dc:date>
    </item>
    <item>
      <title>Re: Using TSS_Library with MQX-Lite</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324201#M14822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;What else should I do to fix this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vinícius Hoff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Aug 2014 12:37:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324201#M14822</guid>
      <dc:creator>ViniciusHoff</dc:creator>
      <dc:date>2014-08-12T12:37:14Z</dc:date>
    </item>
    <item>
      <title>Re: Using TSS_Library with MQX-Lite</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324202#M14823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vinicius:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A time ago I created a MQX-Lite project with TSS Library and the touch slider was not working properly. What I did is to reduce the SysTick timer period to 500 us (Component MQXLite -&amp;gt; Inherited TimerUnit_LDD -&amp;gt; Counter restart -&amp;gt; Period).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not MQX expert, so I don't know all the implications of this change, but at least it worked for my application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Aug 2014 03:09:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324202#M14823</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-08-13T03:09:35Z</dc:date>
    </item>
    <item>
      <title>Re: Using TSS_Library with MQX-Lite</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324203#M14824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the tip, but my touch keys are not working properly yet. I modified the period, but nothing changed.&lt;/P&gt;&lt;P&gt;When I use TSS Library with MQX-Lite project, the interrupt occurs always that I call TSS Task() and each bit of the Faults Register is setted: Charge Timeout, Small Capacitor, Data Corruption, Small Trigger Period and NoiseMode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vinícius Hoff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Aug 2014 21:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TSS-Library-with-MQX-Lite/m-p/324203#M14824</guid>
      <dc:creator>ViniciusHoff</dc:creator>
      <dc:date>2014-08-15T21:12:25Z</dc:date>
    </item>
  </channel>
</rss>