<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックWorkaround for ADC errata e3863 ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Workaround-for-ADC-errata-e3863/m-p/324093#M14802</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear forum members,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i use a K60 ADC in 16bit differential mode with VREFH = 3,3V and VREFL = 0V.&amp;nbsp; The DM-Input is connected to 1,65V (fix voltage) and the DP-Input to our Signal which goes from 0 to 3,3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Errata e3863 says: "DP-Input must be &amp;lt;3,1968V to avoid conversion errors". &lt;/P&gt;&lt;P&gt;So i think i have a problem with the input signal range.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is exchanging DM and DP a possible workaround ? (then DP is fix 1,65V and DM goes from 0V up to 3,3V) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;"e3863: ADC: In 16-bit differential mode, ADC may result in a conversion error when positive input is near upper rail reference voltage Errata"&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"Workaround: To avoid a conversion error near positive full-scale in this mode, do not allow the input voltage on the plus-side of the differential pair (DPx) to exceed (VREFH*31/32)"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Thanks,&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Jul 2014 12:01:48 GMT</pubDate>
    <dc:creator>mikeluetzner</dc:creator>
    <dc:date>2014-07-23T12:01:48Z</dc:date>
    <item>
      <title>Workaround for ADC errata e3863 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Workaround-for-ADC-errata-e3863/m-p/324093#M14802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear forum members,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i use a K60 ADC in 16bit differential mode with VREFH = 3,3V and VREFL = 0V.&amp;nbsp; The DM-Input is connected to 1,65V (fix voltage) and the DP-Input to our Signal which goes from 0 to 3,3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Errata e3863 says: "DP-Input must be &amp;lt;3,1968V to avoid conversion errors". &lt;/P&gt;&lt;P&gt;So i think i have a problem with the input signal range.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is exchanging DM and DP a possible workaround ? (then DP is fix 1,65V and DM goes from 0V up to 3,3V) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;"e3863: ADC: In 16-bit differential mode, ADC may result in a conversion error when positive input is near upper rail reference voltage Errata"&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"Workaround: To avoid a conversion error near positive full-scale in this mode, do not allow the input voltage on the plus-side of the differential pair (DPx) to exceed (VREFH*31/32)"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Thanks,&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jul 2014 12:01:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Workaround-for-ADC-errata-e3863/m-p/324093#M14802</guid>
      <dc:creator>mikeluetzner</dc:creator>
      <dc:date>2014-07-23T12:01:48Z</dc:date>
    </item>
    <item>
      <title>Re: Workaround for ADC errata e3863 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Workaround-for-ADC-errata-e3863/m-p/324094#M14803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Could you tell me the full name of your chip, and the maskset number?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I think it is not only the DP pin should below the &lt;EM&gt; (VREFH*31/32), but also the DM pin should below the &lt;EM&gt; (VREFH*31/32), because in our datasheet, when in 16 bit differential mode, the ADC input voltage should below &lt;EM&gt; (VREFH*31/32)&lt;/EM&gt;.&lt;/EM&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/EM&gt;&lt;/EM&gt; But I will create a project to verify it after you tell me the full name of your chip to see whether my thought is correct.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Of course, you still can verfiy it in you interest in it.&lt;/P&gt;&lt;P&gt;Waiting for your reply!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Aug 2014 07:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Workaround-for-ADC-errata-e3863/m-p/324094#M14803</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2014-08-04T07:56:13Z</dc:date>
    </item>
    <item>
      <title>Re: Workaround for ADC errata e3863 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Workaround-for-ADC-errata-e3863/m-p/324095#M14804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jingjing,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for pointing me to the maskset number. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The full name and maskset nuber of my chip: MK60DN512VLQ10&amp;nbsp; 4N22D&amp;nbsp; QCTCP1411F &lt;/P&gt;&lt;P&gt;I could not see any problems when the input voltage (DP pin) goes over (VREFH * 31/32).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When carefully comparing the erratas it turns out that it applies to 4N30, 2N22D&amp;nbsp; and older but not to the version 2 mask 4N22D we are working with.&lt;/P&gt;&lt;P&gt;Hence, it is not by chance that it works fine with our (newer) processor. Sorry to alert you on this matter and thank you for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;King regards&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mike&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Aug 2014 10:34:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Workaround-for-ADC-errata-e3863/m-p/324095#M14804</guid>
      <dc:creator>mikeluetzner</dc:creator>
      <dc:date>2014-08-04T10:34:11Z</dc:date>
    </item>
    <item>
      <title>Re: Workaround for ADC errata e3863 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Workaround-for-ADC-errata-e3863/m-p/324096#M14805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; That's good to hear that the problem is not exist in your chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Errata 4N22D is really moved the ADC problem, I think the new chip already solved the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Aug 2014 07:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Workaround-for-ADC-errata-e3863/m-p/324096#M14805</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2014-08-05T07:12:38Z</dc:date>
    </item>
  </channel>
</rss>