<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Current consumption on FRDM-KL05</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323808#M14786</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the KL05 is not powered the voltages from the K20 are probably measurable since teh KL05 is not operatimng in a "defined state". This however probably doesn't cause any difficulties when the KL05 is powered normally and in a low power mode since then also the connection pins are defined and so there will be no such "leakage".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jun 2014 12:17:55 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-06-27T12:17:55Z</dc:date>
    <item>
      <title>Current consumption on FRDM-KL05</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323803#M14781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm trying to implement low power modes on KL05 frdm board and measure the current consumption in different modes. Reffering&amp;nbsp; to the schematics, I found out that MCU VDD is connected to P3V3_MCU which is coming from the jumper J4 which is DNP. But a 0 ohm R27 is in parallel to J4. I removed the R27 and soldered a jumper at J4 for putting a multimeter. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But then , what I noticed is MCU is still getting power . I checked the voltage on J4,2 [without putting the jumper], I'm seeing 1.8V. I'm confused from where the voltage is leaking. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anybody faced a similar issue? or am i missing something here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P S : The resistance accross the jumper is 600k ohm&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 07:33:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323803#M14781</guid>
      <dc:creator>pramodtm-b46240</dc:creator>
      <dc:date>2014-06-25T07:33:58Z</dc:date>
    </item>
    <item>
      <title>Re: Current consumption on FRDM-KL05</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323804#M14782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are a number of connections between the KL05 and the Open-SDA interface.&lt;/P&gt;&lt;P&gt;Very probably the you are measuring a voltage derived from there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 19:12:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323804#M14782</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-26T19:12:48Z</dc:date>
    </item>
    <item>
      <title>Re: Current consumption on FRDM-KL05</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323805#M14783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm reffering to FRDM-KL05 schematics. J4.2 is connected to P3v3_MCU which is connected to VDD of MCU. There is no connection between J4.1 and J4.2 . R27 is also removed. So if checked, we can see that MCU VDD is not connected to any pin now. I want to connect the multimeter in ammeter mode between J4.1 and J4.2. But without connecting the MCU is working but at a lower VDD of 1.9V This I'm measuring at J4.2 not anywhere else. I'm suspecting there is a leakage from somewhere to the VDD of MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But can't make out. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2014 05:37:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323805#M14783</guid>
      <dc:creator>pramodtm-b46240</dc:creator>
      <dc:date>2014-06-27T05:37:44Z</dc:date>
    </item>
    <item>
      <title>Re: Current consumption on FRDM-KL05</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323806#M14784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Pramod&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This issue is caused by K20 in SWD still communicates with KL05. So you detect the P3v3_MCU still has voltage value. Hope my reply can resolve your confuse.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2014 07:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323806#M14784</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-06-27T07:12:21Z</dc:date>
    </item>
    <item>
      <title>Re: Current consumption on FRDM-KL05</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323807#M14785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zhe,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for the reply&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Do you mean that since K20 is communicating, I get a voltage on VDD of the MCU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If that is the case, how do you measure current consumption in various power modes?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2014 08:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323807#M14785</guid>
      <dc:creator>pramodtm-b46240</dc:creator>
      <dc:date>2014-06-27T08:12:19Z</dc:date>
    </item>
    <item>
      <title>Re: Current consumption on FRDM-KL05</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323808#M14786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the KL05 is not powered the voltages from the K20 are probably measurable since teh KL05 is not operatimng in a "defined state". This however probably doesn't cause any difficulties when the KL05 is powered normally and in a low power mode since then also the connection pins are defined and so there will be no such "leakage".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2014 12:17:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323808#M14786</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-27T12:17:55Z</dc:date>
    </item>
    <item>
      <title>Re: Current consumption on FRDM-KL05</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323809#M14787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mark,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I just measured the voltage. Since I made out that the MCU is not fully powered off, I didn't continue my experiment on KL05. Shifted to FRDM-KL25. Once, I finish that, I'll start on KL05.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; But, FYI, The MCU is fully powered off when I disconnect the cut trace between jumper pins J4 of FRDM-KL25 unlike on FRDM-KL05 while both use K20 for openSDA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your replies.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2014 13:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Current-consumption-on-FRDM-KL05/m-p/323809#M14787</guid>
      <dc:creator>pramodtm-b46240</dc:creator>
      <dc:date>2014-06-27T13:53:09Z</dc:date>
    </item>
  </channel>
</rss>